2025-08-12 8:48 AM - edited 2025-08-12 9:04 AM
Board/SoC: STM32MP2
Android version: AOSP Android 13 (android-13.0.0_r82)
WebView: com.android.webview 109.0.5414.123 (prebuilt)
Renderer: GLES
Display: 1024×600 (landscape‑native) @ ~63 Hz
Opening an android webview intermittently causes a blank screen. Logs look like the following:
2025-07-30 11:38:13.515 1750-1750 OpenGLRenderer W Surface lost, forcing relayout
The webview never recovers from this state.
Also get the following logs if it is relevant:
2025-08-12 16:16:48.810 3475-3504 OpenGLRenderer E Unable to match the desired swap behavior.
I've also attached the logcat file
Thanks
2025-08-14 1:52 AM
Hi @Jredpath
in Settings->Apps, you can find a "WebView Shell" application. This one works fine on my side.
Currently I don't have strictly the same Android 13 release as you, but we tested "WebView Shell" app before.
Note:
"OpenGLRenderer E Unable to match the desired swap behavior" is not a relevant message, it can be ignored.
BR,
Philippe.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.