2025-04-09 1:13 AM
Hello ST Community,
I'm using the STM32MP257F-DK MPU board and wanted to enable the USART6 interface. We can access it from the 40-Pin GPIO expansion header of the board.
For this, I have enabled the 'status' node settings of the usart6 from the device tree (dts) file as mentioned below.
serial@40220000 {
compatible = "st,stm32h7-uart";
reg = <0x40220000 0x400>;
interrupts-extended = <0x1e 0x1d 0x04>;
clocks = <0x16 0x116>;
dmas = <0x1c 0x13 0x20 0x10012 0x1c 0x14 0x20 0x3021>;
dma-names = "rx\0tx";
access-controllers = <0x1b 0x24>;
power-domains = <0x0c>;
wakeup-source;
status = "okay";
pinctrl-names = "default\0idle\0sleep";
pinctrl-0 = <0x34>;
pinctrl-1 = <0x35>;
pinctrl-2 = <0x36>;
uart-has-rtscts;
phandle = <0xe5>;
};
After setting 'status = okay' in the dts, I'm able to see the '/dev/ttySTM1' device entry on my board on bootup. Now, just to check the uart is enabled or not, I have looped back Tx-Rx pins of the GPIO expansion header and tried to write to the usart (echo "hello" > /dev/ttySTM1") but I see nothing on the console.
I tried to see the clock_summary and found that somehow, the clock status for the usart6 is not enabled. I'm not sure how to enable the clock or what the correct clock_source and clock_id are for this particular usart. [DTS uses clocks = <0x16 0x116>; node for the clock].
root@stm32mp2:~# cat /sys/kernel/debug/clk/clk_summary | grep usart6
ck_icn_p_usart6 0 0 0 200000000 0 0 50000 N deviceless no_connection_id
ck_ker_usart6 0 0 0 64000000 0 0 50000 N serial@40220000 no_connection_id
Tried to enable clock at runtime (Using 'echo on > /sys/class/tty/ttySTM1/device/power/control') for usart6 but it doesn't work. Any thought on how I can enable the usart and get the Tx-Rx loopback working?
Thanks,
Mayank
2025-04-16 7:25 AM
Hello Mayank,
What do you see when typing :
ls /sys/class/tty/ttySTM0/device/driver/?
You should see the base address of the USART6.
Regarding the RIF configuration of the platform. Are the pins of the USART6 (GPIOF13/F14) and the USART6 itself assigned to the Linux kernel? FYI there is a debug entry to check the firewall configuration of the non RIF-aware peripherals (/sys/kernel/debug/stm32_firewall/rifsc).
If all of this is OK, can you make sure that the driver is probed?
Regards,
Gatien
2025-04-16 8:39 AM
Please have a look at https://community.st.com/t5/stm32-mpus-embedded-software-and/stm32mp257-usart-and-serc-exception/td-p/794150 as well.
2025-04-17 2:11 AM
Hello @GatienC ,
Please refer to the following command responses from the development board.
-------------------------------------------------------------------------------------------------------------------
root@stm32mp2:~# ls /sys/class/tty/ttySTM1/device/driver/
400e0000.serial 40220000.serial 40330000.serial bind uevent unbind
root@stm32mp2:~# cat /sys/class/tty/ttySTM1/device/driver/40220000.serial/supplier:platform:44200000.clock-controller/status
active
--> Here, the clock status shows as 'active'.
-------------------------------------------------------------------------------------------------------------------
root@stm32mp2:~# cat /sys/kernel/debug/clk/stm32_clk_summary | grep usart6
ck_ker_usart6 64000000 N
ck_icn_p_usart6 200000000 N
--> Here, It says that the clock is not enabled for usart6.
-------------------------------------------------------------------------------------------------------------------
As you suggested, I have checked if the USART6 is assigned to the Linux kernel or not. From the below command output firewall is disabled so Linux should have access of it.
root@stm32mp2:~# cat /sys/kernel/debug/stm32_firewall/rifsc | grep USART
| USART1 || 31 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |
| USART2 || 32 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |
| USART3 || 33 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |
| USART6 || 36 || NSEC || NPRIV || disabled || disabled || 0 || 0x0 |
-------------------------------------------------------------------------------------------------------------------
You mentioned a similar ticket/thread on the ST forum, Sometime, we are also getting the same exception (Logs below) when trying to access the USART6 (ttySTM1). Stopping the 'st-m33firmware-load.service' helps in this
case.root@stm32mp2:~# echo "test" > /dev/ttySTM1
E/TC:0 stm32_serc_handle_ilac:133 SERC exceptions [63:32]: 0x10
E/TC:0 stm32_serc_handle_ilac:139 SERC exception ID: 36
-------------------------------------------------------------------------------------------------------------------
From our end, We are just shorting Tx-Rx pins (loopback) available on the GPIO header pins and writing (echo "test" > /dev/ttySTM1) to the USART. But we can't see anything coming on the ttySTM1 device.
2025-04-17 6:20 AM
Hello Mayank,
When you disable the M33 firmware, you still get the SERC and nothing on the ttySTM1 device or the SERC occurrences disappear? Can you try to disable the service instead of stopping it? So that the kernel does not launch the M33 Firmware at all.
Cheers,
Gatien
2025-04-20 11:14 PM
Hello @GatienC ,
2025-04-22 5:09 AM
Hi
I don't have a straightforward answer as I'm not an expert of this domain. Maybe someone else from ST or the community is able to answer?
A workaround could be making the USART6 clock critical (CLK_IS_CRITICAL flag to set on this clock) to add to test your functionality.
Cheers,
Gatien
2025-10-23 9:26 PM
Hello @mayank_7117 ,
I could confirm usart3 working well following this way:
1.change linux device tree on usart6 :
Please make sure delete "uart-has-rtscts",change to "status="okay""; add "/delete-property/dmas;" and "/delete-property/dma-names;"
git diff
diff --git a/arch/arm64/boot/dts/st/stm32mp257f-dk.dts b/arch/arm64/boot/dts/st/stm32mp257f-dk.dts
index 88bafebef..952263b8d 100644
--- a/arch/arm64/boot/dts/st/stm32mp257f-dk.dts
+++ b/arch/arm64/boot/dts/st/stm32mp257f-dk.dts
@@ -799,8 +799,9 @@ &usart6 {
pinctrl-0 = <&usart6_pins_a>;
pinctrl-1 = <&usart6_idle_pins_a>;
pinctrl-2 = <&usart6_sleep_pins_a>;
- uart-has-rtscts;
- status = "disabled";
+ /delete-property/dmas;
+ /delete-property/dma-names;
+ status = "okay";
};
2.test method:
Please make sure Cortex-M33 is stopping to void kernel panic.
root@stm32mp2-e3-aa-90:~# echo stop > /sys/class/remoteproc/remoteproc0/state
[ 2055.494747] remoteproc remoteproc0: warning: remote FW shutdown without ack
[ 2055.496198] remoteproc remoteproc0: stopped remote processor m33
root@stm32mp2-e3-aa-90:~# stty -F /dev/ttySTM1 115200
root@stm32mp2-e3-aa-90:~# echo "test" > /dev/ttySTM1 3.Expected result
you will confirm "test" character signal on USART6_TX pin. Please measure USART6_TX pin by oscilloscope or uart-usb converter.
BR,
Yutaka KOTANI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.