2026-04-21 5:49 AM - edited 2026-04-21 5:50 AM
I have an issue were the Linux kernel is booting, then it just stops printing out messages from USART6.
Meanwhile, optee, u-boot and TF-a is printing out messages from USART6. But not Linux after a while.
What can have caused this?
My processor is: STM32MP257F.
2026-04-22 5:52 AM - edited 2026-04-22 7:26 AM
Hello @DMårt ,
Are you sure you don't have a firmware running on M33 that uses or just reconfigure the USART6 instance ? The fact that you have the logs at the beginning but disappear after some time let me think about a such possibility.
[Edit: if not, the USART6 is certainly well configured in earliest boot stages, and Linux does not keep a good configuration on it, but maybe more logs could help to understand exactly where does it disappear]
Kind regards,
Erwan.
2026-04-22 2:11 PM
Here is the log.
As you can see
vddio2: disabling
vddio3: disabling
vddio4: disabling
vddcore: disabling
v1v8: disabling
v3v3: disablingI don't know why this is happening inside Linux.
2026-04-27 5:36 AM - edited 2026-04-27 5:36 AM
Hello @DMårt ,
I think you have a misalignment between your kernel version and your other OpenSTLinux BSP components.
I just felt on this issue by pure chance when working on another topic. It was due to my BSP on OpenSTLinux v6.2 (OP-TEE, TF-A, U-Boot), while my kernel was in OSTL 6.1.
Please double check this.
The blocking point is not the USART at all, but in your complete log, you see the RCC probe is broken:
[ 6.578092] stm32mp25_rcc 44200000.clock-controller: Can't register clk 2: -17
[ 6.583185] stm32 clock failed to initialize
[ 6.587482] stm32mp25_rcc: probe of 44200000.clock-controller failed with error -17
Kind regards,
Erwan.
2026-04-27 7:38 AM - edited 2026-04-27 8:48 AM
Thank you!
It seems that Linux cannot register he HSE clock!!! Or if it's MSI close clock?
I haven't seen that error message! I will look it up. Giving you a reply later.
Edit:
I will look it up what versions I have.
2026-04-27 1:04 PM
Hi again @Erwan SZYMANSKI
I'm using the kernel, TF-a, u-boot and optee from meta-st-stm32mp.
So it's currently version 6.6.78.
Also the firmware for MP2 is 1.3 in CubeMX.
2026-04-28 1:45 AM - edited 2026-04-28 2:18 AM
Hi again @Erwan SZYMANSKI
CLK number n = 2 is the CK_BUS_ETHSW.
See:
https://github.com/STMicroelectronics/linux/blob/v6.6-stm32mp/drivers/clk/stm32/clk-stm32-core.c#L51
https://github.com/STMicroelectronics/linux/blob/v6.6-stm32mp/drivers/clk/stm32/clk-stm32-core.c#L63
Notice:
My Ethernet PHY Realtek is not assembled due to over heating in the ETH PHY (caused by bad soldering). I removed it by using hot air.
But this should not stop Linux to boot I guess?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.