2025-02-07 5:49 AM
Hello,
For students, we recently bought the STM32MP257F eval board, and the related camera and hdmi bridge.
Everything works perfectly and I would like to connect a Raspberry Camera v2. (IMX219) to the board, as it is also a CSI/MIPI camera (and whe have severals).
Can it work ? what should be done related to the software ? (drivers and so on).
By the way, what is the process to install packages in the board ?
Best regards
S. M.
2026-05-13 7:53 PM
Hello,
I also use Raspberry Camera v2. (IMX219) porting on STM32MP257F MPU.
I doubt whether this camera module is compatible with STM32MP257.
This camera can support 8M pixel, but STM32MP257 only support 5M pixel.
Does any one can help me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.