2025-04-25 7:51 AM
Hi, ST Community!
&usb3dr {
status = "okay";
dwc3: usb@48300000 {
maximum-speed = "high-speed";
role-switch-default-mode = "peripheral";
usb-role-switch;
};
};[ 0.085159] usbcore: registered new interface driver usbfs
[ 0.085196] usbcore: registered new interface driver hub
[ 0.085229] usbcore: registered new device driver usb
[ 0.201783] usbcore: registered new interface driver usb-storage
[ 0.202116] usbcore: registered new device driver onboard-usb-hub
[ 0.212602] usbcore: registered new interface driver usbhid
[ 0.212615] usbhid: USB HID core driver
[ 0.300337] scmi-regulator scmi_dev.6: Regulator vdd3v3_usb registered for domain [20]
[ 0.362092] usb-stm32-dwc3 42080000.bus:usb@48300000: configured in usb2 mode
[ 0.365389] usb-stm32-dwc3 42080000.bus:usb@48300000: Enabling runtime PM for inactive device with active children
[ 0.411847] ehci-platform 482f0000.usb: EHCI Host Controller
[ 0.411881] ehci-platform 482f0000.usb: new USB bus registered, assigned bus number 1
[ 0.411994] ehci-platform 482f0000.usb: irq 70, io mem 0x482f0000
[ 0.430691] ehci-platform 482f0000.usb: USB 2.0 started, EHCI 1.00
[ 0.431368] hub 1-0:1.0: USB hub found
[ 0.686236] usb 1-1: new high-speed USB device number 2 using ehci-platform
[ 0.847091] hub 1-1:1.0: USB hub foundSolved! Go to Solution.
2025-05-07 9:47 AM
Hello, @Erwan SZYMANSKI
Thank you for your help and suggestions.
I’ve managed to resolve the issue. The root cause was that I was using a custom Device Tree binary, but it wasn't being properly loaded by U-Boot during the boot process. As a result, the USB gadget was not initialized as expected.
Once I corrected the Device Tree handling in U-Boot and ensured that my custom .dtb was correctly loaded and used during boot, the USB gadget interface (usb0) appeared and started working as intended.
Thanks again for your support!
Best regards,
Nikolai
2025-04-29 2:31 AM
Hello @Nikolai_Navrotski ,
I confirm that in peripheral mode only, M33 FW for Power Delivery is not mandatory (https://wiki.st.com/stm32mpu/wiki/USB3DR_device_tree_configuration#DT_configuration_example_as_USB2-speed_only_USB3DR_in_Peripheral_mode--with_micro-B-28ID_left_unconnected-29_or_Type-C_connector)
Can you give a bit more information concerning the script you launch to configure your USB gadget ?
Kind regards,
Erwan.
2025-04-30 3:02 AM
Hello, @Erwan SZYMANSKI
Thank you for your reply!
We are using script from meta-st-openstlinux without any changes ( https://github.com/STMicroelectronics/meta-st-openstlinux/blob/scarthgap/recipes-bsp/tools/usbotg-gadget-config/stm32_usbotg_eth_config.sh )
Best regards,
Nikolai
2025-04-30 5:20 AM
Hello @Nikolai_Navrotski ,
I took the STM32MP257F-DK board to test the same device tree as you have.
By removing the M33 firmware running, I do not see any issue to make the gadget launch.
Please verify the following points:
Board $> stm32_usbotg_eth_config.sh stop
Board $> stm32_usbotg_eth_config.sh start
Check if you have specific error raised here (module libcomposite not launched for example).
If not, check if you have the usb0 interface up with ifconfig
Be careful, it seems that the default IP address attribution is commented in the gadget script:
interfacename=$(cat ${d}/functions/${func_eth}/ifname 2> /dev/null)
if [ -z "${interfacename}" ];
then
interfacename=usb0
fi
# ifconfig ${interfacename} $IP netmask $NETMASK
ifconfig ${interfacename} up
You can uncomment the line to let the default IP address setting. You can do it manually if you want to set it yourself.
Kind regards,
Erwan.
2025-04-30 9:16 AM
Hello, @Erwan SZYMANSKI ,
Thank you for checking this on the STM32MP257F-DK board and confirming that the gadget should work even without the M33 firmware.
I followed your instructions and verified the following:
I ran stm32_usbotg_eth_config.sh stop and then start — no errors appeared.
The libcomposite module is loaded.
The usb0 interface is up, and ifconfig shows:
usb0 Link encap:Ethernet HWaddr 8E:30:19:40:4E:49
inet addr:192.168.7.2 Bcast:192.168.7.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)However, my host PC still does not detect the USB device at all. There's no new interface or network gadget showing up on the host side.
Could this still be related to some hardware configuration, or USB role settings in the device tree?
Best regards,
Nikolai
2025-05-07 9:47 AM
Hello, @Erwan SZYMANSKI
Thank you for your help and suggestions.
I’ve managed to resolve the issue. The root cause was that I was using a custom Device Tree binary, but it wasn't being properly loaded by U-Boot during the boot process. As a result, the USB gadget was not initialized as expected.
Once I corrected the Device Tree handling in U-Boot and ensured that my custom .dtb was correctly loaded and used during boot, the USB gadget interface (usb0) appeared and started working as intended.
Thanks again for your support!
Best regards,
Nikolai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.