2025-05-13 1:51 AM
Hi,
I am trying to test STM32MP257 hash hardware accelerator according to the following article: https://wiki.st.com/stm32mpu/wiki/Crypto_API_overview.
I was able to utilize the crypto accelerator using openssl (as described in the article), but once I have tried running some tests with SHA-256 hash I have noticed that only software implementation was used. After checking the device tree, I have found that hash accelerator was not enabled. After enabling it and making sure that the kernel driver as also enabled (as module), I am seeing the following error during the boot:
stm32-rifsc 42080000.bus: hash@42010000: Device driver will not be probed
and again, the hash accelerator is not working.
I am running all the tests above on the STM32MP257-DK.
Am I doing something wrong?
Thanks!
Alexey.
2025-05-13 1:58 AM
Hi @altsir_sga
Given the error message I would check the RIFF configuration on Optee device tree side to ensure proper allocation and access right to the CRYP IP from A35.
Hope it help
Olivier
2025-05-13 2:50 AM
Hi Oliver,
After checking the OPTEE device tree, it seems that you are right, the hash accelerator is enabled there and it is locked: RIFPROT(STM32MP25_RIFSC_HASH_ID, RIF_UNUSED, RIF_LOCK, RIF_SEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN).
What is the reason for that? Can I still access it from Linux?
Thanks!
Alexey.
2025-05-13 5:18 AM
Hi,
If you analyze the given RIF configuration that you provided, you can see that the HASH device is assigned to the secure world (RIF_SEC). In order to access it in Linux, you have to assign it to the Cortex A35 non secure:
RIF_SEC=>RIF_NSEC
Other parameter can remain the same.
Here's the documentation for the device-tree bindings of the RIF configuration for the RIFSC in OP-TEE: stm32mp25-rifsc.yaml
FYI, there's a debug entry in the kernel debugfs for you to check the current RIF configuration. Simply enter: cat /sys/kernel/debug/stm32_firewall/rifsc
This will list the configuration of all peripherals that are under the RIFSC.
Some more documentation on the stm32mp2x firewall: https://wiki.st.com/stm32mpu/wiki/STM32MP2_firewall_configuration
I hope this helps,
Gatien
2025-05-13 5:21 AM
For you question: What is the reason for that?
We default assign peripherals related to cryptography to the secure world for the Cortex A35 so that OP-TEE can use them. If you make the change that I proposed above, you'll have to disable the node in OP-TEE's device tree otherwise you'll encounter a similar issue when booting OP-TEE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.