2023-09-26 10:14 AM
Hello, I'm currently working with a STM32MP157D-DK1 Development Board with 4GB DDR3L. I populated the board with a prebuild openstlinux 6.1 build like discribed in a guide in the ST wiki.
When checking the total memory i unfortunatly only get 407MB that are used.
root@stm32mp1:~# free --mega
total used free shared buff/cache available
Mem: 407 138 152 13 140 269
Swap: 0 0 0
Is there a way to use the complete 4GB of RAM?
Kind regards,
Markus
Solved! Go to Solution.
2023-09-27 4:53 AM
HI @MHerz.1 , 407MBytes sound normal. The memory is 4Gbits which is 512MBytes and some part are probably reserved for OpTee, DMA buffers and exchange buffers with Cortex-M4.
Regards
2023-09-27 4:53 AM
HI @MHerz.1 , 407MBytes sound normal. The memory is 4Gbits which is 512MBytes and some part are probably reserved for OpTee, DMA buffers and exchange buffers with Cortex-M4.
Regards
2023-09-27 9:34 AM
Few more details in dmesg
root@stm32mp1:~# dmesg | grep Memory:
[ 0.000000] Memory: 325492K/524288K available (12288K kernel code, 1371K rwdata, 3636K rodata, 1024K init, 235K bss, 133260K reserved, 65536K cma-reserved, 0K highmem)
Maybe look into this page (not fully related, but some interesting information about DDR mapping)
https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_256MB_DDR_mapping_from_STM32_MPU_Distribution_Package#Introduction
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.