2022-10-03 2:09 AM
I'm using a custom board (it is not DK1 even tho it says on boot log) with STM32MP157AAC. The boot hangs on u-boot without proper error message. Where should I start to search the failure?
NOTICE: CPU: STM32MP157AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board - openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
WARNING: regulator_get_by_phandle: phandle 9 not found
WARNING: VDD unknown
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
WARNING: regulator_get_by_phandle: phandle 12 not found
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-1066/888 bin G 2x2Gb 533MHz v1.44
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd9820
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0511570
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc3869
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01ece98
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
ERROR: fixedregulator@3 can not set any flag
WARNING: fixed_regulator_register:81 failed to register fixedregulator@3
NOTICE: SP_MIN: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: SP_MIN: Built : 13:14:26, Nov 23 2021
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: stm32mp1 IWDG1 is secure
INFO: ETZPC: CRYP1 (9) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
U-Boot 2021.10-stm32mp-r1 (Oct 04 2021 - 15:09:26 +0000)
CPU: STM32MP157AAC Rev.Z
Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board - openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
Board: stm32mp1 in trusted mode (st,stm32mp157a-tc1-is-mx)
DRAM: INFO: CPU 0 IT Watchdog 2
INFO: CPU : 0
INFO: sp_usr : 0x0
INFO: lr_usr : 0x0
INFO: spsr_irq : 0x0
INFO: sp_irq : 0x0
INFO: lr_irq : 0x0
INFO: spsr_fiq : 0x0
INFO: sp_fiq : 0x0
INFO: lr_fiq : 0x0
INFO: spsr_svc : 0x0
INFO: sp_svc : 0xc007fe40
INFO: lr_svc : 0xc0144fcd
INFO: spsr_abt : 0x200001d7
INFO: sp_abt : 0xbadc0de
INFO: lr_abt : 0xc010018c
INFO: spsr_und : 0x0
INFO: sp_und : 0x0
INFO: lr_und : 0x0
INFO: spsr_mon : 0x200001d7
INFO: sp_mon : 0x2ffd9e40
INFO: lr_mon : 0xc0100184
INFO: scr : 0x225
INFO: pmcr : 0x41072000
2022-10-11 12:06 AM
@Community member any ideas why the probe fails?
2022-10-11 6:48 AM
no, my only idea was the security configuration
and it seens OK in you test with "DECPROT_NS_R_S_W"
we are using in the STMicroelectronic boards:
DECPROT(STM32MP1_ETZPC_DDRCTRL_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)
DECPROT(STM32MP1_ETZPC_DDRPHYC_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)
and it is enought...
are you sure that the the modified device tree is used in the BL31 SP-MIN on the board ?
I made several timer this error....
no other ideas.
Patrick
2022-10-11 10:12 PM
Yes I'm pretty sure, because this was also my original device tree. I did test it also with buildroot and had the same problem.
2023-02-14 11:16 AM
Wow, I've spent several days debugging it, but this patch has just saved my week!
int dram_init(void)
{
#if 0
...
#else
gd->ram_size = 0x40000000; /* hardcode your DDR size here */
#endif
return 0;
}FTR, I'm upgrading my U-Boot-2020.10-stm32mp-r2 (dunfell) to U-Boot 2021.10-stm32mp-r2 (kirkstone). Without it I was getting following error on DRAM init by u-boot:
ERROR: Illegal access to 0xfdf65fb0:
ERROR: FAIL_ID = 0x4a0
ERROR: Non-Secure
ERROR: Privilege
ERROR: ReadEven though I've got etzpc configured as follows in my tf-a DTS:
DECPROT(STM32MP1_ETZPC_DDRCTRL_ID, DECPROT_NS_R_S_W, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_DDRPHYC_ID, DECPROT_NS_R_S_W, DECPROT_UNLOCK)And memory firewall as default.
@Community member if you have any ideas how to fix that properly, that would be great. I could give a test run on my board if you have any suggestions to test.
Thanks,
Vyacheslav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.