2024-01-16 1:06 AM
Hi everybody,
I'm trying to configure the Wi-Fi module on my custom board (based on the STM32MP153, the Wi-Fi module already tested OK) in Access point mode, and I found the official guide to set hostapd tool to do that:
https://wiki.st.com/stm32mpu/wiki/How_to_configure_a_WLAN_interface_on_hotspot_mode
However, from the tutorial, it seems that hostapd is already installed and preconfigured on the machine, but on my distro (built from st-image-core with openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27) it seems that is not present by default...
How can I add the tool on Yocto layers? Do I have to modify the kernel too? Should be best to add it on my custom/board-specific meta-layer.
Thanks for your time
Solved! Go to Solution.
2024-01-16 3:31 AM
Hi,
From my side, I've added following line in my custom image file:
IMAGE_INSTALL_append = " hostapd"
if you haven't a custom image file, it seems we can do it by adding line in "local.conf" file
Hopes this help
2024-01-16 3:31 AM
Hi,
From my side, I've added following line in my custom image file:
IMAGE_INSTALL_append = " hostapd"
if you haven't a custom image file, it seems we can do it by adding line in "local.conf" file
Hopes this help
2024-01-16 5:00 AM
Hi Eldam,
thanks for the reply! That's exactly what I was looking for, I'll try to include that instruction in my custom image.
I'll set the answer as the solution while I don't find any other problems.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.