2022-07-17 11:20 PM
Hello,
I'm trying to leverage the MCO capability of the STM32MP1, but I don't success. I want to have LSE on MCO1 and HSE on MCO2.
I'm using TFA -> uboot -> linux and I can build with Yocto or Buildroot.
Which steps should be done during TFA, uboot and on Linux ?
I have tried different combination but there is no behaviour.
Also, I'm only doing device tree configuration, maybe I'm missing something elsewhere.
I have seen following resource and I'm confused on the way to proceed because of the warning on MCO pins :
https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
Thanks for your input,
Best regards,
Charles B
Solved! Go to Solution.
2022-07-20 1:41 AM
Hi @Community member ,
Wiith Ecosystem version DV3.x and earlier, CubeMX not handle properly MCO configuration in Uboot and kernel DTS, which lead to a deadlock.
This is what is mentionned as a classical pitfall in https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
From DV4.0 this configuration is properly manage and MCO configuration is done in OPTEE.
If you want to remains in DV3.x or earlier version the w/a consist in using a dummy driver to manage MCO config as per already describe in this post
https://community.st.com/s/question/0D50X0000BDox5VSQR/clock-output-on-mco1-pin-stm32mp157
Hope it help
Olivier
2022-07-20 1:41 AM
Hi @Community member ,
Wiith Ecosystem version DV3.x and earlier, CubeMX not handle properly MCO configuration in Uboot and kernel DTS, which lead to a deadlock.
This is what is mentionned as a classical pitfall in https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
From DV4.0 this configuration is properly manage and MCO configuration is done in OPTEE.
If you want to remains in DV3.x or earlier version the w/a consist in using a dummy driver to manage MCO config as per already describe in this post
https://community.st.com/s/question/0D50X0000BDox5VSQR/clock-output-on-mco1-pin-stm32mp157
Hope it help
Olivier
2022-07-25 2:58 AM
Thanks for your answer. I will check what is the preferred solution in our case.
Regards,
Charles
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.