2026-01-23 6:41 AM
Hello,
I am working with an STM32MP151 and I would like to start the Cortex-M4 core as early as possible during the boot sequence.
The main requirement is to run a real-time task on the M4 that reads an analog input (ANA0 – ADC channel) with minimal startup latency.
In my current setup, the ADC channel is first owned by the Cortex-A7 Linux kernel and is explicitly released and reassigned to the Cortex-M4 via the Linux device tree (by disabling the ADC node for A7 and assigning it to the M4).
Additionally, if I stop the system in boot mode and manually start the Cortex-M4, I am able to successfully debug the M4 firmware and correctly read the ADC value.
My goal is to have the M4 firmware start automatically in the same early boot conditions, without requiring a manual boot/debug sequence.
I would like to understand:
Thank you in advance for your support.
Sabrina
2026-02-02 5:51 AM
Hi @sabry ,
It's possible to start the M4 from U-Boot
Refer to How to start the Cortex-M coprocessor from U-Boot - stm32mpu
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.