2023-03-09 9:36 AM
Hi, we would like to change from 24MHz to 8MHz which is available in our stock, I see in device tree, file stm32mp151.dtsi
clocks {
clk_hse: clk-hse {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <24000000>;
};
.....
I changed clock-frequency = <8000000>;
Is that enough or I do have to set some other config? If there is some other places need to change, could you tell me which ones should be, please?
Solved! Go to Solution.
2023-03-20 9:34 AM
Hi,
This is usually enough... but...
You should adapt some PLL settings due to new HSE frequency.
You must also change USB clock source to PLL4R as 8 MHz is not supported in direct (in CubeMx, USB PLL should receive either precise 19.2, 24, 26, 30 or 38.4 MHz). Changing PLL4 frequency could impact other clocks and so your global clock tree.
I encourage you to use CubeMx to generate the device tree for clocking with HSE = 8MHz.
Regards,
2023-03-20 9:34 AM
Hi,
This is usually enough... but...
You should adapt some PLL settings due to new HSE frequency.
You must also change USB clock source to PLL4R as 8 MHz is not supported in direct (in CubeMx, USB PLL should receive either precise 19.2, 24, 26, 30 or 38.4 MHz). Changing PLL4 frequency could impact other clocks and so your global clock tree.
I encourage you to use CubeMx to generate the device tree for clocking with HSE = 8MHz.
Regards,
2023-03-21 6:34 AM
Yes, I use STM32CubeMX generate the clock configuration and get it working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.