2025-04-03 4:09 AM
The kernel is complaining that the specified root partition (identified by the PARTUUID) is not found or isn’t valid, and this is happening at the kernel level rather than in U‑Boot. In other words, U‑Boot is simply passing the kernel command line (which includes something like:root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582) to the kernel, and then the Linux kernel itself is trying to locate that partition during its mounting phase.
please find the boot logs attached.
2025-04-03 4:11 AM
I'm using SanDisk Micro SD/SDHC 32GB Class 10 Memory Card (Ultra).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.