2020-01-27 7:42 PM
Have been spending time reading the Wiki about the Yocto environment, is there a link to forward technical suggestions and grammar corrections?
2020-02-05 1:02 AM
Hi @KevinA
This Q&A section is the right place to do so.
Thanks to share your suggestions/corrections in a dedicated post.
BR,
Olivier
2020-02-07 10:30 PM
Finally received the new computer, while setting up I found the 'Get Started' needs a link to Development zone/PC prerequisites
After installing everything from Development zone/PC prerequisites I started the Getting started where the first issue was the java 8 install, Development zone/PC prerequisites installed java 11 (sudo apt install default-jre). Next came the STMCubeProgrammer v2.2.0 which is now 2.3.0 and when you run the setup it installs in $HOME/STMicroelectronics/STM32Cube/STM32CubeProgrammer and nothing in the WiKi matches what v2.3 just did...
I added export PATH=$HOME/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin:$PATH to my .bashrc and tested the programmer, ok. The next 'step' was copying the rules so I copied the *.rules since they don't need Readme.txt and version.txt in the /etc/udev/rules.d directory. I think I picked up on everything, I did not install Android, that comes after I get the distribution setup so we can see if our application will run.
Will continue tomorrow - FYI it appears Development zone/PC prerequisites installed everything yet 4.2 USB serial link has me installing again.
2020-02-08 3:55 PM
I started back up this morning but had to stop:
403
Forbidden
Here are some suggestions:
From the Getting Started:
3 Download the SDK
3.1 For ecosystem release v1.1.0
Link: (20 directories below the root of the website, it may have broke from all the pressure at that depth)
I gave it a while and just tried again, nope, still broke.
You really should have a site crawler going to prevent this from causing customer grief
2020-02-08 8:57 PM
403
Forbidden
Here are some suggestions:
From the Getting Started:
3 Download the SDK
3.1 For ecosystem release v1.1.0
Link: (20 directories below the root of the website, it may have broke from all the pressure at that depth)
2 Download the the Linux® kernel source code
2.1 For ecosystem release v1.1.0
403
Forbidden
Here are some suggestions:
I'll move/copy these to a post in the main MP1 forum, nothing is happening here
Basically, if we can't download the files we are just wasting time.
2020-02-09 11:00 PM
Sunday morning the problem was still there and I did some global traceroutes, then IP Whois to discover two groups claiming the IP address, Amazon and cscglobal.com. I sent an email to cscglobal.com letting them know about the issue and by noon it appears to have been resolved. I downloaded the current Source and installed it completing the WiKi to they part of installing the IDE BUT the Wiki doesn't have STM32CubeIDE, Why? I downloaded from st.com and installed but how do I hook into STM32MPU?
The Wiki needs an update starting with the STM32Programmer, no GUI to the install, the SDK has been updated and the source has changed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.