2021-02-10 1:54 AM
We are using STM32MP157c-DK2 board. Using STM32MP_KeyGen_CLI tool generated public key, private key and publicKeyhash.bin.
As mentioned in STM32 webpage, https://wiki.st.com/stm32mpu/wiki/KeyGen_tool
Hash public key contains the SHA-256 hash of the public key in binary format which generated by Gen tool.
Is there a way or steps to generate same publicKeyhash.bin (without using STM32 key_Gen tool) via openssl or any other crypto utility
2021-02-24 7:45 AM
Hi @Rajesh Kannan Selvam ,
I recover this draft / not verified procedure in case it can help and give some pointers :
To generate the header, you need to follow the format given by the wiki https://wiki.st.com/stm32mpu/wiki/STM32_header_for_binary_files
The key and signature are stored in a raw binary format.
To extract raw public key from .pem file, I suggest you use the pycryptodome python module (https://pypi.org/project/pycryptodome/ ; https://pycryptodome.readthedocs.io/en/latest/, https://pycryptodome.readthedocs.io/en/latest/src/public_key/ecc.html)
First, use an openssl command to convert your .pem file into a .der one (pycryptodome doesn’t accept .pem files)
openssl ec -in privateKey.pem -outform der -out privateKey.der
Then, use this script as example:
-----------------------------------------------------------------------
from Cryptodome.PublicKey import ECC
def dump_buffer(buf,step=16,name=""):
print("%s (%d bytes):" % (name, len(buf)))
for i in range(0,len(buf),step):
print (" ".join(["%02X" % c for c in buf[i:i+step]]))
f = open('privateKey.der','rt')
key = ECC.import_key(f.read())
pubk = key.public_key()
dump_buffer(pubk.pointQ.x.to_bytes(),name="x")
dump_buffer(pubk.pointQ.y.to_bytes(),name="y")
from Cryptodome.Hash import SHA256
from Cryptodome.Signature import DSS
message = b'I give my permission to order #4355'
h = SHA256.new(message)
signer = DSS.new(key, 'fips-186-3')
signature = signer.sign(h)
dump_buffer(signature,name="signature")
-----------------------------------------------------------------------
Hope it help
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.