2020-07-23 9:24 AM
I'm trying to connect to my DK2 from STM32CubeIDE but the ST LInk port doesn't seem to work. In Device Manager I see "Unknown USB Device (Device Descriptor Request Failed)". I tried several cables and ports on my PC.
I should mention that I'm running a minimal Ubuntu but used the kernel from the ST build process, I just swapped out the rootfs with the Ubuntu version.
When I switch back to the stock SD card image the port shows up as VID/PID 0x1D6B/0x0104 but I can't install any drivers for it.
How does whatever I program into the SD card affect how the ST Link USB port shows up?
Thanks,
ANdrew
Solved! Go to Solution.
2020-07-23 10:21 AM
Never mind - I had the wrong port! I thought the DFU port was used for ST-Link when the DIP switches were the other way. It works now with the micro-USB connector.
Andrew
2020-07-23 10:21 AM
Never mind - I had the wrong port! I thought the DFU port was used for ST-Link when the DIP switches were the other way. It works now with the micro-USB connector.
Andrew
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.