2021-06-03 12:08 PM
Hi, ST :)
In addition to https://community.st.com/s/question/0D53W00000pUh4gSAC/tfa-and-uboot-custom-compile-fails
Could you plese explain me what is the reason for such error:
dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!
while downloading flash content with CubeMXProgrammer.
I've built a core image with bitbake st-image-core command (hope I'm correct here) and got UBI image with size 116Mb (121896960b). I'm expecting it can be fitted to a UBI partition that has size 0x07a00000b = 127926272b. Please refer to nand partition table below. spi-nand flash size is 128Mb.
TF-A and u-boot was manually build during duscussion mentioned with link above.
Here is .tsv file:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32
- 0x03 fip-boot Binary none 0x0 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x04 fsbl Binary(2) spi-nand0 0x000000 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-nand.stm32
P 0x05 fip1 Binary spi-nand0 0x200000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x06 fip2 Binary spi-nand0 0x400000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x10 UBI Binary spi-nand0 0x600000 ./st-image-core-openstlinux-weston-stm32mp1-duck_nand_4_256_multivolume.ubi
Here is exact console output:
Here is console full output while CubeMX programming (one more question after log):
-----------------------
NOTICE: CPU: STM32MP157DAB Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):
NOTICE: BL2: Built : 13:28:40, Jun 2 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :0, Manifestation 0 at c00001dc
INFO: phase ID :3, Manifestation 3 at c80feb64
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
WARNING: Image id=31 size out of bounds
ERROR: BL2: Failed to load image id 31 (-27)
NOTICE: CPU: STM32MP157DAB Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):
NOTICE: BL2: Built : 13:28:40, Jun 2 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :0, Manifestation 0 at c00001dc
INFO: phase ID :3, Manifestation 3 at c80f9ea3
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd847c
WARNING: Not a known TEE, use default loading options.
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0512a91
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc4258
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01cfa18
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.4-r1.0(debug):
NOTICE: SP_MIN: Built : 15:20:23, Jun 2 2021
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: ETZPC: UART1 (3) could be non secure
INFO: ETZPC: SPI6 (4) could be non secure
INFO: ETZPC: CRYP1 (9) could be non secure
INFO: ETZPC: I2C6 (12) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
U-Boot 2020.10-stm32mp-r1 (Jun 02 2021 - 18:21:14 +0300)
CPU: STM32MP157DAB Rev.Z
Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
Board: stm32mp1 in trusted - stm32image mode (st,stm32mp157a-stm32mp151-dk1-mx)
DRAM: 512 MiB
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
In: serial
Out: serial
Err: serial
invalid MAC address in OTP 00:00:00:00:00:00
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!adc_measurement: single shot failed for adc@0[18]!
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.
Hit any key to stop autoboot: 0
Boot over usb0!
partitions : done
DFU alt info setting: using id 'spi-nand0,0'
using id 'spi-nand0,1'
using id 'spi-nand0,2'
dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!
Error: dfu init failed: -1
done
STM32MP> mtdparts
device spi-nand0 <spi-nand0>, # parts = 4
#: name size offset mask_flags
0: fsbl 0x00200000 0x00000000 0
1: ssbl1 0x00200000 0x00200000 0
2: ssbl2 0x00200000 0x00400000 0
3: UBI 0x07a00000 0x00600000 0
active partition: spi-nand0,0 - (fsbl) 0x00200000 @ 0x00000000
defaults:
mtdids : spi-nand0=spi-nand0
mtdparts: mtdparts=spi-nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)
-----------------------
BTW, I'm also not able to load 0x04,0x05,0x6 partitions without specifying 0x10 partition with following error:
Boot over usb0!
Error: fip2 (0x6): Bad size for partition 3 (ssbl2) at 0x400000 = 0x7c00000 <> 0x200000 expected
Here is .tsv (last line is commented):
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32
- 0x03 fip-boot Binary none 0x0 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x04 fsbl Binary(2) spi-nand0 0x000000 ./tf-a-stm32mp157a-stm32mp151-dk1-mx-nand.stm32
P 0x05 fip1 Binary spi-nand0 0x200000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x06 fip2 Binary spi-nand0 0x400000 ./fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
#P 0x10 UBI Binary spi-nand0 0x600000 ./st-image-core-openstlinux-weston-stm32mp1-duck_nand_4_256_multivolume.ubi
This migh be convinient for TF-A/U-BOOT debugging - no need to wait for download huge images...
Thank you for your patience :)
Looking forward for your reply
Solved! Go to Solution.
2021-06-07 9:40 AM
2021-06-07 5:40 AM
Hi @ASkri.1 ,
Sorry I'm not expert of nand and mtd but the mention trace
dfu_fill_entity_mtd: Memory layout (/0x10/1*122Me) not supported!
looks to be obvious
Look inside u-boot source "drivers/dfu/dfu_mtd.c"
if ((!strcmp(st, "part")) || (!strcmp(st, "partubi"))) {
...
}
else {
printf("%s: Memory layout (%s) not supported!\n", __func__, st);
return -1;
}I understand you provide one parameter as "/0x10/1*122Me" where it expect to find "part" or "partubi"
Hope this help
Olivier
2021-06-07 9:40 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.