2024-02-13 1:12 PM - edited 2024-02-13 1:14 PM
Please show me a working example of setting up the MMU for STM32MP157D-EV1. and where to place the Translation table correctly (for cortex A7)
It is assumed that all data and program will be located in DDR memory, without using the OS
2024-02-13 11:32 PM
MMU settings are automatically handled by our OpenSTLinux deliveries. You don't have (and you can't) setup it directly.
If you are playing bare-metal, please note that STMicroelectronics did not provide any bare-metal support on STM32MP15 series. You have to check with ST partners https://www.st.com/content/st_com/en/partner/partner-program.html?key=STM32MP&country=country#2 .
Nevertheless, as we provide bare-metal support on STM32MP13 series thru STM32CubeMP13 delivery.
https://www.st.com/en/embedded-software/stm32cubemp13.html
As this device use same Cortex-A7 (but single core only) and very close HW, maybe you could get some insight from this delivery.
Regards
2024-02-14 8:16 AM - edited 2024-02-14 8:53 AM
The latest version of StmCubeMX does not correctly create a project for stm32mp13 bare-metal (for STM32MP135F-DK)
there is no .cproject file with environment settings, as well as a linker file
The set of files that created the StmCubeMX
./mmu_test
./mmu_test/.mxproject
./mmu_test/Application
./mmu_test/Application/Core
./mmu_test/Application/Core/Inc
./mmu_test/Application/Core/Inc/cortex.h
./mmu_test/Application/Core/Inc/gpio.h
./mmu_test/Application/Core/Inc/main.h
./mmu_test/Application/Core/Inc/RTE_Components.h
./mmu_test/Application/Core/Inc/stm32mp13xx_hal_conf.h
./mmu_test/Application/Core/Inc/stm32mp13xx_it.h
./mmu_test/Application/Core/Src
./mmu_test/Application/Core/Src/cortex.c
./mmu_test/Application/Core/Src/gpio.c
./mmu_test/Application/Core/Src/irq_ctrl_gic.c
./mmu_test/Application/Core/Src/main.c
./mmu_test/Application/Core/Src/mmu_stm32mp13xx.c
./mmu_test/Application/Core/Src/stm32mp13xx_hal_msp.c
./mmu_test/Application/Core/Src/stm32mp13xx_it.c
./mmu_test/Application/Core/Src/system_stm32mp13xx_A7.c
./mmu_test/Drivers
./mmu_test/Drivers/CMSIS
--skip--
./mmu_test/Drivers/STM32MP13xx_HAL_Driver
--skip--
./mmu_test/mmu_test.ioc
./mmu_test/STM32CubeIDE
./mmu_test/STM32CubeIDE/.project
./mmu_test/STM32CubeIDE/.settings
./mmu_test/STM32CubeIDE/.settings/org.eclipse.core.resources.prefs
--end--
2024-02-14 10:57 PM
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.