2024-07-31 3:56 AM
Dear,
I'm starting with OP-TEE on STM32MP15x line. I bring-up the board as described here and built the optee_example_hello_world as described here. However, I got the error code below:
TEEC_Opensession failed with code 0xffff0008 origin 0x3
Checking the boot messages, I realized that the profile system_services is used. This way, it is not possible to run any TA.
So, is there any already compiled image for STM32MP157C-DK2 board that allows running a TA or do I have to modify the image to enable it?
Thanks!
Solved! Go to Solution.
2024-08-08 6:55 AM
2024-07-31 12:57 PM - edited 2024-07-31 12:58 PM
Hello @Charles Dias ,
Since OSTL v5.0, OP-TEE default configuration is non secure and loaded into DDR. It is mentioned here in OP-TEE overview : https://wiki.st.com/stm32mpu/wiki/OP-TEE_OTP_overview#OP-TEE_OS_configuration
So no, unfortunately we do not have an already compiled image that does what you want. You will have to recompile some components to load OP-TEE in SYSRAM, and activate secure_and_system_services profile.
Kind regards,
Erwan.
2024-08-06 5:00 AM
Hi, @Erwan SZYMANSKI,
When I activate the secure_and_system_services profile, should I load the OP-TEE in SYSRAM or can I keep it on DDR even if it's not secure?
Thanks for your help!
2024-08-06 5:10 AM
Hello @Charles Dias ,
Yes you need to put OP-TEE in SYSRAM on MP15 because this is the only memory secured for this series.
On MP13, you can put OP-TEE in DDR for this same use case.
Kind regards,
Erwan.
2024-08-08 6:55 AM
Solution described in this post:
2024-08-11 8:33 AM
Yes you need to put OP-TEE in SYSRAM on MP15 because this is the only memory secured for this series.
For MP1 there are two modes and I managed to run them both:
1. With secure OP-TEE in SYSRAM and paging in DDR:
2. With unsecure OP-TEE in DDR
2024-11-18 2:25 AM
hello.
Sorry if I intrude on this post. It's not a relevant topic. I don't know who to turn to. I'm new to the forum and I need a little help.
I'm preparing the stm32mp157c-dk2 board with yocto project mickledore.
I have a problem compiling my Yocto for stm32mp157c-dk2 project. I run the bitbake command from build "bitbake -e core-image-minimal".
I get the error message: Error, the PACKAGE_ARCHS variable (all any noarch ${PACKAGE_EXTRA_ARCHS:tune-cortexa7}cortexa7 stm32mp157c_dk2) for DEFAULTTUNE (cortexa7) does not contain TUNE_PKGARCH ().Toolchain tunings invalid:
Tuning 'cortexa7' has no defined features, and cannot be used.
I tried to solve without success.
Anyone know how to solve it?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.