2021-09-03 3:27 AM
Hi all,
I am trying to achieve DDR data transfer between M4 and A7.
So I followed How to exchange data buffers with the coprocessor - stm32mpu article and built a yocto image.
I have stripped down the logic analyzer application : here .
I have few questions of concerns:
In case of the CM4 code provided here : Link
There no support in the latest cube-mx to create an RPMSG_HDR_HandleTypeDef type object which might be labelled as /dev/tpmsg-sdb type in user space application.
Although the data structure is similar to VIRT_UART_HandleTypeDef. So I went ahead and made and rpmsg-sdb object of the later type.
Now when I run my stripped down application part of attached zip. I get below error on A7-console :
CA7 : Forward efd info for buf0 with mFdSdbRpmsg:5 and efd:6
./backend: failed to set efd: Inappropriate ioctl for deviceNote that now I get 3 devices : ttyRPMSG0 , 1 , 2. So in order to identify which is the sdb one I initialized it at the last in M4 code. Not sure if that is right way.
Kindly advice what might be potential root cause of issue here.
Solved! Go to Solution.
2021-09-03 6:26 AM
Update : Never mind. Solved it. There was a minor change in the CM4 project, where in there was an extra file set : rpmsg_hdr.c / .h was created to handle the data transfer over rpmsg-sdb channel. After making those changes in the CM4 side. Seems to work now perfectly.
2021-09-03 5:56 AM
Update : Looks like the stm32_rpmsg_sdb driver gets loaded , but there is no device called : /dev/rpmsg-sdb which shows up.
2021-09-03 6:26 AM
Update : Never mind. Solved it. There was a minor change in the CM4 project, where in there was an extra file set : rpmsg_hdr.c / .h was created to handle the data transfer over rpmsg-sdb channel. After making those changes in the CM4 side. Seems to work now perfectly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.