2022-04-16 4:04 PM
This is my current cursor.json file
{
"device": "/dev/dri/card0",
"outputs": [
{ "name": "HDMI-A-1", "mode": "1024x600", "size": "1024x600" }
],
"hwcursor": false
}Here are my env Qt variables
QT_QPA_EGLFS_ALWAYS_SET_MODE=1
QT_QPA_EGLFS_INTEGRATION=eglfs_viv
QT_QPA_EGLFS_KMS_CONFIG=/usr/share/qt5/cursor.json
QT_QPA_PLATFORM=eglfs
QT_QPA_EGLFS_KMS_ATOMIC=1But when I try to run any Qt application I get this
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
EGLFS: Failed to open /dev/fb0
EGLFS: Can't continue without a display
Aborted (core dumped)I have verified that /dev/fb0 does not exist, and /dev/dri/card0 does.
Finally, here is my modetest output, and reason why I have cursor.json file as it is.
...
Connectors:
id encoder status name size (mm) modes encoders
33 32 connected HDMI-A-1 470x260 10 32
modes:
index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
#0 1024x600 59.82 1024 1068 1156 1344 600 603 609 625 50250 flags: phsync, nvsync; type: preferred, driver
...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.