STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The question about STM32MP157CAC3 supply

Hello. I have used the STM32MP157A-DK1 this year and I have learned to work with it. Now I develop my own PCB with STM32MP157CAC3. There is a 12-V external power supplier in it. I do't use USB Type-C. Can I do like this? I care about pins USB_PWR_CC1...

DFomi.1 by Associate II
  • 3190 Views
  • 5 replies
  • 0 kudos

glib meson error: ERROR: <ExternalProgram 'python3' is not a valid python or it is missing setuptools

I have been trying to compile an image in Yocto with a custom machine to load my own device tree, but when trying to compile I always get the same error, here is a log: Log data follows:| DEBUG: Executing shell function do_configure| gtkdocize: neith...

FPini.1 by Associate II
  • 5745 Views
  • 7 replies
  • 0 kudos

STM32MP1 bRIGUP watchdog trip

HI. I have a custom board that basically identical to the PDKWe Made 2 Boards for test.One starts up OKThe Other failsSection of Console belowThe section of interest is the lineINFO:  CPU 0 IT Watchdog 2 and soThe Same SDCard in both.Must be a hardwa...

Bkell.1 by Associate II
  • 5208 Views
  • 3 replies
  • 0 kudos

Resolved! The problem with facilitating uboot errors

When compiling the U-boot, these four commands are used:PC $& gt; export KBUILD_OUTPUT=.. /build/stm32mp15_trustedPC $& gt; export DEVICE_TREE=stm32mp157c-dk2PC $& gt; make stm32mp15_trusted_defconfigPC $& gt; make alluse the first: export KBUILD_OUT...

Ffu.1 by Associate II
  • 4850 Views
  • 4 replies
  • 0 kudos

Resolved! How to configure HDMI in openstlinux_eglfs st-example-image-qt image running on STM32MP157C-DK2

I need to connect a Waveshare Electronics 5.5" HDMI AMOLED display that does not provide it's supported modes, their website states it needs to be configured manually with the followingmax_framebuffer_height=1920max_usb_current=1config_hdmi_boost=10h...

PWilk.2 by Associate II
  • 4467 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.