2022-11-09 6:33 AM
After following the wiki page "how to create your board device", I am exactly in the situation indicated at the end of this page : "The execution should fail just after the "Booting BL32" notice, because state definitions are missing in the device tree (in the pwr node overlay)".
For information, I don't use the Yocto (layers etc) env and the full OpenSTLinux distrib, but rather a custom buildchain and the ***-stm32mp-r2 sources (TF-A 2.4, U-boot 2020.10 & linux 5.10 with lightened conf). All of this works well on the EV-1 board using the associated ST conf (dts etc.) and I am now trying to port all that on a custom board.
In my porting task, I am then guessing the next step is to add custom-made conf in device trees, especially the pwr node. I would get inspiration from the EV-1 dts but my custom board does not have a PMIC as our stm32mp151 doesn't need to manage low power modes (which should make it more simple?), among other little differences.
Where could I find ressources / doc / training / guides/ examples of those next steps of board-specific configurations (pwr, rcc, clk...) ?
I think the AN5256 "discrete power supply" will help me along the way, as well as the embedded documentation in the source packages, but these are much less beginner-friendly than the wiki.st.com how-to guides.
2022-11-14 9:14 AM
Hi @Théo Tourrès
maybe this post might help you as pointing some places of examples of discrete power device tree.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.