2020-02-11 5:33 AM
Hi ,
I am working with STM32MPU DK2 and Distribution package and have some of basic queries.
1.1how do i know which device tree .dts is used ?
1.2 if i execute a new project from cubeMX it generates project skeleton and a .dts file, shoud i have to rebuild linux with this .dts?
1.3 On runtime, can i get to know if a particular peripheral is assigned a particular processor?
2. I have obtained the terminal of the board using Minicom and i m able to execute the programs on Linux A7 and M4 using the below links...
But how can i crossverify if M4 is what is being executed or other?
3. Where can i find the source code for AI demo from the Linux environment? or any demo that contains source files of both the processors application?
Background: Trying to establish a communication between A7 and M4 using RPMsg mechanism.
Thanks in Advance
Vivek
2020-02-11 6:04 AM
Hi @Vthul
Did you browse the wiki user guide ?
https://wiki.st.com/stm32mpu/wiki/Resource_manager_for_coprocessing
In CubeMX, Pinout&Configuration pane you have option "show context" accessible from the parameter wheel on top of peripheral list.
1.1how do i know which device tree .dts is used ?
on target look at /boot/extlinux/extlinux.conf file to see dts mapping with start menu selection.
1.2 if i execute a new project from cubeMX it generates project skeleton and a .dts file, shoud i have to rebuild linux with this .dts?
Yes you have to rebuild the dts generated by CubeMX.
See
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package
or
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
1.3 On runtime, can i get to know if a particular peripheral is assigned a particular processor?
Check for IP status in cat /proc/device-tree/soc/ (CA7) and cat /proc/device-tree/m4@0/m4_system_resources/ ( CM4)
eg for a timer assigned on CM4 :
root@stm32mp1:cat /proc/device-tree/soc/timer@40000000/timer\@1/status
disabled
root@stm32mp1:cat /proc/device-tree/m4@0/m4_system_resources/timer@40000000/status
okay
2. I have obtained the terminal of the board using Minicom and i m able to execute the programs on Linux A7 and M4 using the below links...
But how can i crossverify if M4 is what is being executed or other?
see https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview
3. Where can i find the source code for AI demo from the Linux environment? or any demo that contains source files of both the processors application?
Background: Trying to establish a communication between A7 and M4 using RPMsg mechanism.
To start experiment communication between A7 and M4 using RPMsg mechanism I suggest you start by looking at the exemple OpenAMP_TTY_Echo provided in STM32MP1 Cube Package
see https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_Package
Hope it help
BR,
Olivier
2020-02-11 7:08 AM
Hi Oliver,
Thanks a lot for the detailed answer.
Will check and update.
Viveknath
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.