2024-01-05 2:17 AM - last edited on 2024-01-05 2:20 AM by Peter BENSCH
Getting panic error during optee binary update. We are stuck on this. Kindly provide any guidance.
We are using emmc for boot and Two file updating till now. But after fip-stm32mp135f-dk-optee.bin update we are getting this error. Here is the log-
NOTICE: CPU: STM32MP135F Rev.Y
NOTICE: Model: STMicroelectronics STM32MP135F-DK Discovery Board
INFO: PMIC version = 0x21
INFO: Reset reason (0x35):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):()
NOTICE: BL2: Built : 17:16:39, Jan 4 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-1066 bin F 1x4Gb 533MHz v1.53
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: handle USB : Suspend int
INFO: USB Suspend mode
INFO: handle USB : Reset
INFO: phase ID :3, Manifestation 0 at c717367e
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x30006000
INFO: Image id=1 loaded: 0x30006000 - 0x30006236
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x30006000
INFO: FCONF: Reading firmware configuration information for: mce_config
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde000000
INFO: Image id=8 loaded: 0xde000000 - 0xde07b3a8
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0400000
INFO: Image id=2 loaded: 0xc0400000 - 0xc040f8f0
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0000000
INFO: Image id=5 loaded: 0xc0000000 - 0xc00e866c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde000000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Embedded DTB found
I/TC: OP-TEE version: Unknown_3.19 (gcc version 12.2.0 (GCC)) #1 Fri Jan 5 09:42:01 UTC 2024 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: WARNING: All debug access are allowed
E/TC:0 0 Panic at core/arch/arm/plat-stm32mp1/drivers/stm32mp1_pmic.c:183 <initialize_pmic_i2c>
E/TC:0 0 TEE load address @ 0xde000000
E/TC:0 0 Call stack:
E/TC:0 0 0xde0030f9
E/TC:0 0 0xde019f73
E/TC:0 0 0xde00683d
E/TC:0 0 0xde018b85
E/TC:0 0 0xde018c55
E/TC:0 0 0xde01933f
E/TC:0 0 0xde01ac61
E/TC:0 0 0xde002fbb
E/TC:0 0 0xde00019c
2024-02-01 11:28 PM
I have the exact same issue with PB7 and PE15. Have you been able to solve this issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.