2020-09-09 1:17 AM
Hi all,
Windows 10 IoT Core already supports run on the single ARM Cortex-A7 MPU! Is there a BSP of the STM32 MPU that can be used for the Windows 10 IoT?
Refer here:
https://docs.microsoft.com/en-us/windows/iot-core/learn-about-hardware/socsandcustomboards
Best Regards
2020-09-25 8:05 AM
Hi @yanming2013 mo
In case in may fit your need we are supporting Microsoft AZURE IoT
Please refer to :
https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_integrate_Azure_IoT_Edge_on_OpenSTLinux
Olivier
2020-09-26 2:14 AM
Hi @Community member ,
Thanks for your reply.
The Azure IoT is totally not the same as the windows 10 IoT.
The Windows 10 IoT is a kind of OS that will instead of the Windows CE. The Azure IoT is a kind of the component and needs run on some OS like Windows 10 IoT or Linux.
As I knew that, the windows 10 IoT already supports the single-core of ARM Cortex-A7 and the STM32MP1 already can be supported by the Windows 10 IoT, but the BSP of the STM32MP1 should be supported by your team.
Please refer here to get more information about the windows 10 IoT and BSP:
https://docs.microsoft.com/en-us/windows/iot-core/windows-iot-core
https://docs.microsoft.com/en-us/windows-hardware/manufacture/iot/create-a-new-bsp
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.