2021-07-05 4:22 AM
Hi all,
I am trying to bring a LVDS display up. Display: BOE EV121WXM-N10-1850. Datasheet: Link
Driving MPU : STM32MP1. I am using VisionSoM STM32MP1 based evaluation Kit. Link
The firmware changes required to make the device up are part of git: Link
I have made following changes in the dts files to support display:
kernel/stm32mp157a-visionsom-rgb-emmc-mx.dts and u-boot/stm32mp157a-visionsom-rgb-emmc-mx.dts has following changes :
panel {
compatible = "boe,ev121wxmn10", "simple-panel";
backlight = <&backlight>;
port {
panel_in: endpoint {
remote-endpoint = <<dc_out_rgb>;
};
};
};In case u-boot/stm32mp157a-visionsom-rgb-emmc-mx-u-boot.dtsi
panel {
display-timings {
timing0: timing0 {
clock-frequency = <74250000>;
hactive = <1280>;
vactive = <800>;
hfront-porch = <48>;
hback-porch = <80>;
hsync-len = <32>;
vback-porch = <15>;
vfront-porch = <3>;
vsync-len = <5>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <0>;
pixelclk-active = <1>;
};
};
};Here i have added panel settings to support the above display. Now the port which i have out on the board is RGB. I have used RGB to LVDS converter DS90C385A. Since I am trying to drive LVDS display.
The issue i am facing is that , I am unable to drive the display. Nothing is coming up.
Queries:
Solved! Go to Solution.
2021-07-06 3:01 AM
Hi,
I'm not specialist, maybe asking Somlabs could be useful for support on their DT.
Probably missing some <dc node modifications to define that the panel is connected to it.
Example with external si9022 RGB2HDMI transceiver could be helpful : https://wiki.st.com/stm32mpu/wiki/LTDC_device_tree_configuration
Regards,
2021-07-06 3:01 AM
Hi,
I'm not specialist, maybe asking Somlabs could be useful for support on their DT.
Probably missing some <dc node modifications to define that the panel is connected to it.
Example with external si9022 RGB2HDMI transceiver could be helpful : https://wiki.st.com/stm32mpu/wiki/LTDC_device_tree_configuration
Regards,
2021-07-07 2:11 AM
Thanks @PatrickF for the response , will take a look into it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.