2020-08-07 12:56 AM
Hi
i have a ltdc tft display RGB parallel display connected to stm32mp15 series,
unable t0 get drm link to DPI connector, the code flow is breaking at following files,
using
DISTRO = "openstlinux-weston"
i have no idea where to start to debug
linux-4.19.49/drivers/gpu/drm/drm_modes.c
if (mode->flags & ~DRM_MODE_FLAG_ALL)
return MODE_BAD;--- failing here not moving further
DTS:
panel_rgb: panel-rgb {
compatible = "okaya,rs800480t-7x0gp";
status = "okay";
dvdd-gpios = <&gpioc 13 GPIO_ACTIVE_HIGH>;
avdd-gpios = <&gpiod 7 GPIO_ACTIVE_HIGH>;
cs-gpios = <&gpioa 12 GPIO_ACTIVE_HIGH>;
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_mp1som_pins_a>;
pinctrl-1 = <<dc_mp1som_sleep_pins_a>;
port {
panel_in_rgb: endpoint {
remote-endpoint = <<dc_out_rgb>;
};
};
};
<dc {
status = "okay";
port {
#address-cells = <1>;
#size-cells = <0>;
ltdc_out_rgb: endpoint@0 {
reg = <0>;
remote-endpoint = <&panel_in_rgb>;
};
};
};
weston.ini:
[output]
name=HDMI-A-1
mode=1280x720
# DSI connector
[output]
name=DSI-1
mode=preferred
transform=270
attached is the drm log
2020-08-07 10:16 PM
as a update , when i remove the validation check, i could able to see a continious RGB and black white test pattern is seen on the LCD tft
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.