2021-07-22 3:31 AM
Hi,
I am trying to develop something around the STM32MP1.
For that I have made some changes in the dts file via cubeMx and followed the process of building it given here.
What is the location where the dtb file generated ? My arch/arm/boot/dts folder looks empty.
Is there something i am missing?
executing make dtbs seperately also exits cleanly but does not generated the dtb file.
2021-07-22 5:14 AM
Hi,
Once generated, .dtb should be in $WORKDIR/kernel/build/arch/arm/boot/dts/ .
Assuming custom kernel .dts files has been copied in $WORKDIR/kernel/kernel-sources/arch/arm/boot/dts/ .
Here is the commands I use (which are aligned with https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#Updating_the_kernel_device_tree)
export WORKDIR=$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0
pushd $WORKDIR/Developer-Package
source SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
popd
pushd $WORKDIR/kernel/kernel-sources
make ARCH=arm O="$PWD/../build" multi_v7_defconfig fragment*.config
for f in `ls -1 ../../sources/arm-ostl-linux-gnueabi/linux-stm32mp-*/fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
yes "" | make ARCH=arm oldconfig O="$PWD/../build"
make stm32mp157f-custom-mx.dtb LOADADDR=0xC2000040 O="$PWD/../build"
popd
ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/stm32mp157f-custom-mx.dtbIf not working as expected, please carefully double check if you have followed :
Then, if no .dtb is generated, there is maybe an error messages issued during one process.
.dtb make should output something like (if .dts has been touch):
make[1]: Entering directory '/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/kernel/build'
SYNC include/config/auto.conf.cmd
GEN Makefile
DTC arch/arm/boot/dts/stm32mp157f-custom-mx.dtb
make[1]: Leaving directory '/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/kernel/build'Regards,
2021-07-22 5:17 AM
Hi @NPal.2
If you are following https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Modifying_the_Linux_kernel_device_tree this section assume you are using the "Inside kernel source tree directory" methods .. to the opposite of the "outside kernel source tree" which generate all build artefacts in a specific "build" directory.
Please check which configuration is active when calling "make dtbs".
refer to https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt for full details procedure of kernel build .
Hope it help
Olivier
2021-07-22 6:53 AM
@Community member @PatrickF :Thanks for the response let me try this and get back.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.