cancel
Showing results for 
Search instead for 
Did you mean: 

kernel log "/cpus/cpu@0 missing clock-frequency property" on stm32mp151C

JSand.10
Associate

We are running a stm32mp151c with stm32mp linux built with yocto.

The kernel complain that the cpu0 clocl-frequency is not set, but the patch

layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp/5.10/5.10.116/0022-ARM-5.10.116-stm32mp1-r2.1-DEVICETREE.patch removes DTS clock-freuency setting

line 3889: -         clock-frequency = <650000000>;

From release notes STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu for 5.15 I found "BL2 always boots at 650MHz" and it seems the kernel should probe for cpu clock-frequency. The board boots, but we get these log entries that makes me wonder if we miss anything in DTS:

"Starting kernel ...

[  0.003140] /cpus/cpu@0 missing clock-frequency property

[  2.666366] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517"

Could anyone give me a hint where I can find more info about this patch and the background for removing the DTS cfg line "clock-frequency = <650000000>" but still code want to find DTS cfg please? I understand the opp should replace this but can both be used at the same time?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Olivier GALLIEN
ST Employee

Hi @Johan Sandström​ ,

I understand you are in kernel 5.10 / V3.x ... Pay attention to refer to the relevant wiki

stm32mpu-ecosystem-v3

Anyway the traces you report are simple warning that can be ignore in this version.

They are removed in V4.x / kernel 5.15

Hope it help,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JSand.10
Associate

Thanks a lot! I will look at the patches for 4.X .

debugging
Lead

These are traces in 6.1

[ 0.000000] OF: fdt: Machine model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
[ 0.000000] printk: bootconsole [earlycon0] enabled
[ 0.003370] /cpus/cpu@0 missing clock-frequency property
[ 0.008773] /cpus/cpu@1 missing clock-frequency property

debugging
Lead

This warning went away by adding the cpu frequency in the DTS.  (ECO 5.0. , kernel 6.1). CubeMX did NOT add those.

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.