2023-11-03 2:09 AM
Hi
I see the STM32MP135 has an ISO7816 interface. Have you developed a compatible Linux device driver for the ISO7816 interface? There exist a software framework to use the SAM (Secure Module Access) Card connected to this interface?
Thank you,
2023-11-07 4:53 AM
ISO7816 is supported in UART STM32 driver from V5.0.0 release but there is no framework in Linux to use it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.