2021-06-03 11:44 PM
2021-06-04 12:44 AM
Note that SDMMC3 (together with other interfaces which could be useful for a WiFi+BLE module like UART SAI, etc...) is available on GPIO expansion connector of STM32MP157D-DK1 (the one without 1DX module nor display as probably useless for your trials) or STM32MP157F-EV1.
I think this could be handy for modules evaluation (using direct wiring or a small custom PCB).
If you need high-speed and good signal integrity on SDMMC3, DK1 would be recommended as wires to GPIO expansion are shorter than EV1 board.
Regards.
2021-06-03 11:59 PM
Hi @KK.4 ,
No we only offer Discovery and Evaluation boards.
What would you expect from a Nucleo ? Is it a matter of price or functionalities ?
Thanks,
Olivier
2021-06-04 12:02 AM
Thanks for the quick reply.
We wanted to have the functionality, as we would like to test the board with different communication modules of our choice.
2021-06-04 12:04 AM
Hi,
there is no plan to offer a Nucleo for MPU products.
Depend on your needs, STM32MP157x-DK1/DK2 board offer Arduino as well a general purpose IO connector (similar to the one on well known fruit-named board)
Nevertheless, there is plenty of 3rd party offering with STM32MP1 series which could be similar to a Nucleo (small size, reduced peripheral set and optimized cost).
or simply search on the web for "STM32MP1 module"
Regards.
2021-06-04 12:23 AM
Thanks for your reply. The intention here is to evaluate different communication modules (Wi-Fi + BLE) with STM32MP1 host, having the flexibility of a Nucleo setup. I could see that the development board is already equipped with Wi-Fi + BLE combo module 1DX from Murata, interfaced over SDIO. I would like to test STM32MP1 with a different Wi-Fi module of choice but didn't want to start the development from scratch.
2021-06-04 12:44 AM
Note that SDMMC3 (together with other interfaces which could be useful for a WiFi+BLE module like UART SAI, etc...) is available on GPIO expansion connector of STM32MP157D-DK1 (the one without 1DX module nor display as probably useless for your trials) or STM32MP157F-EV1.
I think this could be handy for modules evaluation (using direct wiring or a small custom PCB).
If you need high-speed and good signal integrity on SDMMC3, DK1 would be recommended as wires to GPIO expansion are shorter than EV1 board.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.