2019-10-07 9:45 PM
2019-10-08 11:56 AM
Hi @Jzhua
Yes OpenSTLinux Weston can be used without GPU.
Using Distribution package if you reject the GCNANO licence agreement during configuration, you will have an automatic fallback to Weston display path not using GPU.
Hope it help
Olivier
2019-10-08 9:56 PM
I just see the need to accept the eula. Do I need to say no? Like this
Do you accept the EULA you just read? (y/n) n
[WARNING] Configure build without support of packages under EULA acceptance.
2019-10-10 1:46 AM
Yes that's it.
Note that further adaptation may have to be done in the boot chain and Kernel Device Tree.
Using STM32CubeMX is recommended to help writing them.
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.