2025-05-25 4:09 AM
I am about to integrate Ezurio sna module If 513 with the STM32MP257F-EV another to provide wireless capabilities to my board. does any one try this before for any assistance. I am using mini PCIE TO M.2 adapter to connect. so if there is any to assist me with a complete guide , I will appreciate,
Thank you.
2025-05-25 5:49 AM
Have you already set up Linux on the board? If you plug the module into the miniPCIe and run lspci, will it show up?
2025-05-25 6:18 AM
the only thing I see is 00:00.0 PCI bridge: Synopsys, Inc. Device 0550 (rev 01)
2025-05-25 12:18 PM
And you see the same without the module connected (and powered up)?
Can you connect the module to some other host system and compare results?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.