2019-06-30 8:46 PM
Any recommendations on how to install Node.js on OpenSTLinux / OpenEmbedded?
I want to run some node.js applications on the A7 processor.
I found this repository but there has been no activity for a few years.
2019-08-28 2:56 AM
I have generated image with bitbake st-example-image-qt command after added nodejs to local.conf .
However, after added meta-iot-cloud to local.conf with CORE_IMAGE_EXTRA_INSTALL += "packagegroup-cloud-google", it gives the following erros;
ERROR: nodejs-native-8.12.0-r0 do_compile: oe_runmake failed
ERROR: nodejs-native-8.12.0-r0 do_compile: Function failed: do_compile (log file is located at /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/x86_64-linux/nodejs-native/8.12.0-r0/temp/log.do_compile.28025)
2020-01-14 1:26 AM
Hi,
Sorry for late reply.
Applying attached patch 0001-nodejs-bump-to-10.16.2 in Distribution package might fix the compilation issue by getting a more recent nodejs version.
apply patch 0001-nodejs-bump-to-10.16.2.patch on meta-st-openstlinux
put the following line on conf/local.conf
PREFERRED_VERSION_nodejs = "10%"
PREFERRED_VERSION_nodejs-native = "10%"
and you must have:
$> bitbake -s | grep node
nodejs :8.12.0-r0 :10.16.2-r0
nodejs-native :8.12.0-r0 :10.16.2-r0
Olivier
2020-02-26 2:28 AM
As a workaround you could try to run node in a container with supported used land, It would require meta-virtualization with a couple of patches, like this one:
2022-04-26 3:41 AM
Hello community,
I'm trying to implement node.js in distribution package for STM32MP157F-DK2. I'm little new to this development. I'm facing few issue after adding node.js from https://github.com/imyller/meta-nodejs
I'm getting a error when I'm trying t build:
ERROR: Nothing RPROVIDES 'meta-nodejs' (but /home/radesh/STM32MPU_workspace/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'meta-nodejs' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['meta-nodejs']
ERROR: Required build target 'st-image-weston' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-image-weston', 'meta-nodejs']Steps I follow:
cd layers
git clone https://github.com/imyller/meta-nodejs
bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-nodejsI have created a file called "nodejs_%.bbappend" with these contents
EXTRA_OEMAKE += "builddir_name=."
in this directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/recipes-devtools/nodejs
and added a stanza to
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/conf/layer.conf
to include nodejs
IMAGE_INSTALL_append += "nodejs"
After this all I try to build using:
bitbake st-image-weston
Thanks in advance for your valuable answers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.