2019-06-15 5:24 AM
Is STM32MP157C source code support for STM32MP151A processor , if so please provide appropriate link .
Thanks,
Nitish
2019-06-16 11:17 PM
Hello,
you need to get the developer package, see https://wiki.st.com/stm32mpu/wiki/Which_Package_better_suits_your_needs#Developer_Package
2019-06-17 10:39 PM
Yea, Thanks for replaying PatrickF , the developer package which you have sent consists of STM32MP157 dts file, is it support for STM32MP151 development board
If it does not can you provide links of STM32MP151A
Regards, Ntish
2019-06-17 11:49 PM
Hello,
we only provide boards with STM32MP157A or C, so dts in developer package are aligned to this boards.
dts files aligned to other devices and specific development board should be generated using STM32CubeMx (need to be tailored manually for completeness regarding detailed board/peripherals settings).
See https://wiki.st.com/stm32mpu/wiki/How_to_assign_an_internal_peripheral_to_a_runtime_context
2019-06-18 4:13 AM
Hello,
Thanks for suggesting and I am able to get the dts for STM32MP151AAD3 from STM32CubeMX, so I am re asking question like can I get kernel and U -boot for this board and even tool chain also?
Regards, Nitish
2019-06-18 5:14 AM
Hello Nitish, The source code delivered by ST is compatible with all the chips and all the boards provided by ST. This is the same Source code and toolchain. So you can get it from the developer package or the distribution package.
2019-06-18 10:47 PM
Thanks for replaying Bernard PUEL, I can able to get kernel , U-boot and also SDK. from developer package link,https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1dev.html,
as per the README doc of U-boot, can build the source with 157 dts but how can compile the 151 dts which is generated by STM32CubeMX with this source code ?
2019-06-19 2:03 AM
Ok I catch it. You will generate your 151 mx dts (with your board config) then you just need to copy these dts in your build (for TF-A, U-Boot or Kernel).
See the structure and how to do this in this article:
https://wiki.st.com/stm32mpu/wiki/STM32MP15_device_tree#STM32CubeMX_generated_device_tree
2019-06-20 10:07 PM
Thanks for support, I can able to compile the kernel with generated dts file using def file name "multi_b7_defconfig" but if I try to compile using "stm32_defconfig", getting errors, so what is difference between these two def config, which def config need to use for our board STM32MP151A compilation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.