cancel
Showing results for 
Search instead for 
Did you mean: 

How to use the RTL8723BU in "Ecosystem V2.0.0"?

Machilus
Associate III

Hi All

​If you create a distribution with RTL8723BU enabled in the Linux kernel and boot, you will see the error message below.

[  30.102790] usb 2-1.2: 1f8: ff ff ff ff ff ff ff ff

[  30.106213] usb 2-1.2: RTL8723BU rev E (SMIC) 1T1R, TX queues 3, WiFi=1, BT=1, GPS=0, HI PA=0

[  30.118408] usb 2-1.2: RTL8723BU MAC: 34:c9:f0:8d:fc:72

[  30.124300] usb 2-1.2: rtl8xxxu: Loading firmware rtlwifi/rtl8723bu_nic.bin

[  30.131982] usb 2-1.2: Direct firmware load for rtlwifi/rtl8723bu_nic.bin failed with error -2

[  30.141236] usb 2-1.2: request_firmware(rtlwifi/rtl8723bu_nic.bin) failed

[  30.146569] usb 2-1.2: Fatal - failed to load firmware

[  30.155477] rtl8xxxu: probe of 2-1.2:1.2 failed with error -11

If you search for the "rtl8723_nic.bin" file on the entire Linux system, it doesn't exist.

Is there any other way to use RTL8723BU in "Ecosystem V2.0.0"?

The method shown on the ST WiKi site is not a solution as it assumes that the device driver is loaded normally.

Any suggestions on how to solve the above problem would be appreciated.

Thanks and regards

Machilus

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Machilus
Associate III

Hi all.

I partially solved this problem.

It can be solved by taking the "rtl8723bu_nic.bin" file from the realtek git site and putting it in the "/lib/firmware/rtlwifi" folder.

However, when the Bluetooth and Wi-Fi functions are used together, one side of the Wi-Fi or Bluetooth is disconnected.

I'm looking for a solution to that problem. If you know anything that could be a hint, let me know.

Thanks and regards

Machilus

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.