STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[stm32mp1] Multiple ttyRPMSG

Hi, I have a STM32MP157F-DK2 with a firmware running with remoteproc and using remoteproc and rpmsg drivers to communicate with userspace through ttyRPMSG0, created at firmware init with libmetal and openAMP libraries. After multiple days of research...

Resolved! STM32MP1 - Bare metal on A7

Hi,I have a current project using the M7 that I need to port over to the A7. The goal is to be running bare-metal code on the A7, like we are on the M7. Currently, I am following this open source guide to run bare-metal on the A7 and it seems to work...

mkurtz by Associate II
  • 6052 Views
  • 6 replies
  • 0 kudos

Resolved! STM32MP1 ETH_PHY_INTN

Hello! I am developing a custom board based on STM32MP151C MPU (TFBGA 361pins) with a RMII Ethernet PHY, and I have a simple question regarding to the PHY interrupt signal -sorry if this is a duplicated question, I haven't found a related topic in th...

jmglez by Associate
  • 2616 Views
  • 2 replies
  • 0 kudos

Resolved! Can't run st-example-image-qt QT examples on a custom board based on STM32MP153C with RGB panel

I'm trying to run QT examples on a build created using st-example-image-qt (Ecosystem v2.1) on our custom board. We have a simple RGB display 800x480 resolution, so I modified the cursor.json on the board as follows{ "device": "/dev/dri/card0", "outp...

NBhat.1 by Associate III
  • 4316 Views
  • 5 replies
  • 0 kudos

Resolved! STM32MP157: CAN does not receive anything

Hello,I am using a STM32MP157C development board from Myirtech and trying to interface the board with a CAN device.I am able to bring up the can0 interface. It can send data, I can see it from oscilloscope over Can Hi and Lo pins. The dmesg output is...

mertt by Associate II
  • 3170 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.