2020-11-12 7:22 AM
I would syncrhonize A7 and M4 on STM32MP151A using IPCC interrupt, how can I do it?
Moreover, using FreeRTOS, I need to start some task before of MX_OPENAMP_Init, but I noticed if I move this function after the Kernel starting, it doesn't work. I don't understand why?
2020-11-17 2:16 AM
Have you tried to use OpenAMP examples provided inside the STM32Cube_FW_MP1 software package release? (Application/OpenAMP). Some examples are given to exercise FreeRTOS and OpenAMP which initialises/configures IPCC events.
Here's the entrypoint. https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_Package
2020-11-20 2:23 AM
Hi Olivier,
thank you for the response.
I looked to entrypoint but it doesn't resolve my troubles. Due to in Openamp init the rproc_virtio_wait_remote_ready is blocking until Linux wakes up and due to some functionalities need to start before of Linux, I would manage the init of library in a separate task while another task containing the cited functionalities runs without waiting Linux.
I noticed that I moved the openamp initialization when Linux starts this task is blocked on waiting yet while the others starts fine, but I don't understand the reason of that. Is it possible that starting the FreeRTOS kernel before the OpenAmp init then it changes some memory areas where M4 expects to read the status from A7? How can I do it?
2020-11-20 5:29 AM
Hi GNapo.1 (Community Member)
It seems that your are experiencing a similar issue as described in the following post:
https://community.st.com/s/question/0D53W000004l5HJ/openamp-hangs-at-mxopenampinit-when-started-from-uboot-even-after-waited-for-linux-to-fully-booted-up
Could you please have a look at it and let me know if it solves your problem?
Best Regards,
Olivier
2020-11-24 4:01 AM
Hi Oliver,
thank again. I saw the post but resource table is found, but investigating I noticed that in the MX_OPENAMP_Init function it returns -1 after executing
vdev = rproc_virtio_create_vdev(RPMsgRole, VDEV_ID, &rsc_table->vdev,
rsc_io, NULL, MAILBOX_Notify, NULL);
if (vdev == NULL)
{
return -1;
}
It is strange because the function seems is not able to allocate dynamically vdev. How it is possible?
I have scheduled the MX_OPENAMP_Init inside StartDefaultTask
defaultTaskHandle = osThreadNew(StartDefaultTask, NULL,NULL);
Best Regards,
Giuseppe
2020-11-30 6:49 AM
Hi @OlivierK ,
do you have news for about that?
Thank you in advance.
King Regards
2020-12-02 3:42 AM
Hi GNapo.1 (Community Member),
I am not able to reproduce. It seems your having an issue during the memory allocation . Have you tried to increase the heap/stack config sizes?
Kind Regards.
2020-12-02 3:45 AM
Hi Olivier,
thanks.
Do you mean heap\stack of FreeRtos or in linker file of M4?
King Regards.
2020-12-02 9:53 AM
Hi GNapo.1 (Community Member)
The problem may come from the allocated shared memory for OPENAMP defined in the linker file.
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000298
m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000
m_data (RW) : ORIGIN = 0x10020000, LENGTH = 0x00020000
m_ipc_shm (RW) : ORIGIN = 0x10040000, LENGTH = 0x00008000
}
As in the OpenAMP_FreeRTOS_echo example, can you make sure you haven't modified this?
Kind Regards
2020-12-03 2:42 AM
Hi @OlivierK ,
this is my linker file
/* Highest address of the user mode stack */
_estack = 0x10040000; /* end of RAM */
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */
/* Memories definition */
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000298
m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000
m_data (RW) : ORIGIN = 0x10020000, LENGTH = 0x00020000
m_ipc_shm (RW) : ORIGIN = 0x10040000, LENGTH = 0x00008000
}
/* Symbols needed for OpenAMP to enable rpmsg */
__OPENAMP_region_start__ = ORIGIN(m_ipc_shm);
__OPENAMP_region_end__ = ORIGIN(m_ipc_shm)+LENGTH(m_ipc_shm);
Today I will try to increase the heap\stack size as you said in the previous response. I will give you a feedback.
King Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.