2021-08-02 8:09 AM
Hello,
I am having difficulties with the MMC bus and the external SDIO wifi module. We are using the wifi module jody-w263 from U-blox with the OSD32MP1, and the communication with the module works, but it is quite slow. The wifi module is capable of SDR 104 and DDR50 communication speeds, but I add the support to the DTS, the communication is broken and the device returns the -110 while initializing.
How can I add support for higher speeds?
I attach the working dts, dmesg, ios and caps, and relevant schematic.
Any suggestion will be appreciated.
Best regards,
Tomáš.
Solved! Go to Solution.
2021-10-20 10:21 PM
2021-10-20 11:49 PM
Hello Tomas,
I see this trace:
[ 3.273770] mmci-pl18x 48004000.sdmmc: mmc_regulator_set_vqmmc: found vmmc voltage range of 3300000-3400000uV
Are you sure you have "vqmmc-supply = <&v1v8_ldo1>;" in your devicetree ?
2021-10-21 12:20 AM
Hello,
yes, this line is there. I am attaching the dts file, that is in the yocto build directory (i.e. <yocto_build>/tmp-glibc/work/stm32mp157c_tevogs_v3_mx-ostl-linux-gnueabi/linux-stm32mp/5.4.56-r0/linux-5.4.56/arch/arm/). I also attach the decompiled dts that I took from the build dir and the dtb itself so you can check it. The v1v8_ldo1 regulator has the phandle number 0x2b and the same value is referenced in the vqmmc-supply of the sdmmc@48004000 node.
p.s.: in the decompiled file I had found the max-frequency is 120 Mhz, so I guess it is the default value, if not specified in the dts.
2021-10-21 5:41 AM
2021-10-21 6:14 AM
2021-10-21 7:38 AM
2021-10-21 7:39 AM
2021-10-21 8:16 AM
2021-10-21 11:25 PM
2021-10-22 12:28 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.