2024-11-12 9:15 PM
I am trying stm32mp157f-dk2 for learning linux based on starter package
I just got succeed with load example 1 dtb and echo uart operating
Anyway so I got checked the extlinux.conf file can control which dtb would be called
But I dont know what's happening let me show what i wonder
1. Why stm32mp157c-dk2-extlinux.conf is called?
2. Why load stm32mp157c-dk2.dtb? there's not FDT setting in default LABEL
I can do with just change conf file in 157c-dk2 for now
But i want to know how to select conf file
Thank you
2025-01-12 6:20 AM
Hi, I have similar problem to understan extlinux.conf file.
I built and flash image to my STM32MP157f-dk2 board. The next I edited *.dts file by adding m_can1 , I am compiled *.dts file to *.dtb and copy to target board to /boot directory .... I Restart board and still I do not have CAN device....
I thinking that problem is related which *.dtb called..
@SKim.1761Do you tried change *.dts file adding any interface ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.