2022-07-19 3:53 PM
Is HAL_UARTEx_ReceiveToIdle_DMA supported on STM32MP15 products? If so is there an example for using it?
2022-07-20 11:31 PM
Hi @cfilipescu ,
The CubeMP1 HAL does not contain HAL_UARTEx_ReceiveToIdle functions, but you could easily reuse them from CubeH7 which share almost same UART/USART HW.
See also this H7 post which also link to an interesting page: https://github.com/MaJerle/stm32-usart-uart-dma-rx-tx#idle-line-or-receiver-timeout-events
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-08-12 5:52 AM
Not a concrete example so I can't select it as best answer.
2022-08-12 6:34 AM
And also see this link to understand how ridiculous and incompetent the HAL API design is...
2022-08-12 5:03 PM
I'd imagine anything you engineer will be better than anything in, or missing, from the deeper HAL implementation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.