2022-08-12 12:10 AM
Hello,
When I tried using fseek and getc functions for my project the MP1 failed to execute their code. The execution stops at lines that contain __IO_acquire_lock(fp) and __IO_need_lock(fp) macros and then terminates in the fseek and getc functions respectively. I also tried other file handling functions such as fread and fwrite and they also fail. Is there anyway to solve this issue?
thanks for any answers
Solved! Go to Solution.
2022-08-15 2:49 AM
I was able to solve the issue by using the arm-linux-gnueabihf-gcc and scp commands to compile the code and send it to the MP1 rather than using STM32CubeIDE to do those things.
2022-08-15 2:49 AM
I was able to solve the issue by using the arm-linux-gnueabihf-gcc and scp commands to compile the code and send it to the MP1 rather than using STM32CubeIDE to do those things.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.