2020-08-15 11:44 AM
I'm bringing up a custom STM32MP15x-based design, and I'm encountering what looks like stack corruption issues in U-Boot (and I can't get a kernel to boot).
Symptoms:
I've enabled early debug printing, and get the following output:
U-Boot SPL 2020.04-stm32mp-r1 (Aug 15 2020 - 13:11:31 -0500)
Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.45
Trying to boot from MMC1At this point, the console hangs for a really long time. Looking at the UART on a logic analyzer, I see that during this time, it's printing seemingly gibberish characters at 1750 baud (which my USB-to-serial converter is ignoring due to the framing errors caused by the wrong baud).
I did some brief JTAG investigations, and somewhere along the way, something calls printf() on a character buffer that's corrupted (so it doesn't encounter a null-terminating character for a very, very, very long time).
Eventually, it will print something like this:
▒▒*aQ▒rrr▒In: serial
Out: serial
Err: serial
Enter fastboot!
invalid MAC address in OTP 00:00:00:00:00:00
board_check_usb_power: Can't get adc device(-19)
Net: No ethernet found.
No USB device found
USB init failed: -19
Hit any key to stop autoboot: 0
Boot over mmc0!
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Unknown command 'test▒t▒▒t▒▒▒t▒▒▒' - try 'help'
Found /boot/extlinux/extlinux.conf
Retrieving file: /boot/extlinux/extlinux.conf
131 bytes read in 18 ms (6.8 KiB/s)
1: stm32mp157a-dk1-buildroot
Retrieving file: /boot/zImage
4158848 bytes read in 200 ms (19.8 MiB/s)
append: root=/dev/mmcblk0p4 rootwait
Retrieving file: /boot/stm32mp157a-dk1.dtb
44188 bytes read in 19 ms (2.2 MiB/s)
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
Loading Device Tree to cfff2000, end cffffc9b ... OK
Starting kernel ...At this point, it hangs and doesn't do anything else.
Sometimes it finds all the environmental variables and attempts to boot the kernel, sometimes it doesn't. Either way, it often complains about bad filesystems, gibberish character names for things, etc.
I can poke around with my J-Link some more, but it looks like RAM is corrupted.
However, after enabling the (supposedly fancier) new memtest in buildroot, I tested 0xC0000000 to 0xDD000000 for hundreds of iterations without a single reported problem (If I test higher than that, I think I start running into U-Boot).
About the board:
My goal is to to throw together the simplest break-out board possible, so I've got VDD_CORE and VDDQ_DDR tied to a 1.35V 2A buck converter, and VDD at 3.3V via a 600 mA LDO. I'm using the internal 1.8V, 1.1V, and 1.2V regulator. I'm using the STM32MP157A-DK1 U-boot / DTS config, modified to eliminate the PMIC. I have the identical Micron memory part mounted to the board.
Known issues
Any ideas of where to look next? Because the DRAM seems to check out, I'm thinking it's a power delivery issue. I've added quite a bit of bulk capacitance (five or six 10 uF caps) around the processor and RAM, but that doesn't seem to do much of anything.
Solved! Go to Solution.
2020-09-14 10:52 PM
@SMich.1, as I said, I'm not using a PMIC — just 3.3V and 1.35V regulators.
By the way, I ended up solving the problem! I had swapped DQM0 and DQM1 (ugh). Since 90% of U-Boot uses 32-bit accesses, it actually kind-of-sort-of worked, but it would glitch out whenever there was an 8-bit access. That's also why the memtest passed with flying colors (since it also uses 32-bit accesses). I did a bit of PCB surgery to swap the signals and now the board boots up and runs without issues.
2020-08-24 7:57 AM
Hi @Community member
Could you precise with with ecosystem version you are working ? V1.2 ( kernel 4.19) or V2.0 ( kernel 5.4) ?
I remind you that in V2.0 ( kernel 5.4) we removed basic boot support ( start kernel for U-boot spl).
Also there is dependance between tf-a, uboot which require to use all component from V2.0.
For hardware perspective I would recommend, if possible, to contact a local ST FAE for more efficient support.
Hope it help
Olivier
2020-08-26 1:43 PM
Honestly, I'm just using whichever versions of U-Boot / Linux that are currently in Buildroot. I forgot to mention that this SD card boots fine on a DK1 board, so it's definitely a hardware issue. Thanks for the help anyway, though.
2020-08-28 2:10 AM
Which PMIC do you have 1A , 1B? because my board manufacturer said that he can't get the 1A version and on B you have different ranks for the power up that could made problems with power up sequence.
you can burn the NVIC memory to make it like 1A version like in DK1 board .
2020-09-14 10:52 PM
@SMich.1, as I said, I'm not using a PMIC — just 3.3V and 1.35V regulators.
By the way, I ended up solving the problem! I had swapped DQM0 and DQM1 (ugh). Since 90% of U-Boot uses 32-bit accesses, it actually kind-of-sort-of worked, but it would glitch out whenever there was an 8-bit access. That's also why the memtest passed with flying colors (since it also uses 32-bit accesses). I did a bit of PCB surgery to swap the signals and now the board boots up and runs without issues.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.