2022-12-21 6:54 AM
Hi!
I am using a STM32MP157C-DK2 board to communicate via CAN. To do this, I have created a program in STM32CubeIDE and set the FDCAN parameters:
I have been testing in engineering mode and I was able to receive and send CAN messages (I have connected to an IXXAT device).
My problem starts when I try to do it in production mode:
I do not know if I forgot to set a clock or something to enable FDCAN.
Can someone help me please?
Thanks!
2022-12-21 8:05 AM
Hi @TArre.1
Root clocks (i.e. PLLs, mux) and power supplies are managed by uBoot/Linux.
In order to control them properly, the Device Tree should contain resources required by your Cortex-M4 FW. Also, the resource manager should be enabled.
These are usually configured within CubeMx.
See https://wiki.st.com/stm32mpu/wiki/How_to_configure_system_resources
and https://wiki.st.com/stm32mpu/wiki/Resource_manager_for_coprocessing
and https://wiki.st.com/stm32mpu/wiki/How_to_assign_an_internal_peripheral_to_a_runtime_context
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-12-22 3:20 AM
Hi @PatrickF , thank you for your reply!
I have created the device tree in CubeMx. After reading all the wiki pages, i have verified in my program the following parameters (kernel .dts):
m4_fdcan1_pins_mx: m4_fdcan1_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 11, RSVD)>, /* FDCAN1_RX */
<STM32_PINMUX('A', 12, RSVD)>; /* FDCAN1_TX */
&m4_m_can1{
pinctrl-names = "default";
pinctrl-0 = <&m4_fdcan1_pins_mx>;
status = "okay";
&m4_rproc{
m4_system_resources{
status = "okay";
&m4_m_can1{
pinctrl-names = "default";
pinctrl-0 = <&m4_fdcan1_pins_mx>;
status = "okay";
I think I have all the parameters set correctly. Is there any other step I have to do?
Thanks!
2022-12-22 11:31 PM
Hi,
note that clocks should be defined in TF-A DT (as well as in uBoot and linux kernel DT).
Check if fdcan_k is from right source: cat /sys/kernel/debug/clk/clk_summary
If not, check if DT is what you expect for FDCAN_CK, e.g. https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.6-stm32mp/fdts/stm32mp15xx-dkx.dtsi#L254
Check in your DT that you did not have status = "okay" on &m_can1 node.
Check in your M4 code that you skip the right init when in production mode but still have somewhere a code that enable the FDCAN clocks, e.g. __HAL_RCC_FDCAN_CLK_ENABLE().
Check in your M4 code that you still have GPIO mux for FDCAN pins.
Regards
2022-12-25 2:34 PM
hi @PatrickF
In order to change the clocks, do I have to create my own machine?
I have checked the clocks with the command "cat /sys/kernel/debug/clk/clk_summary" and I have seen that the configuration is not the same as the one I have designed in the STM32CubeIDE:
clock enable_cnt prepare_cnt rate accuracy phase
----------------------------------------------------------------------------------------
clk-hse 1 1 24000000 0 0
ck_hse 7 7 24000000 0 0
ck_hse_rtc 0 0 1000000 0 0
stgen_k 1 1 24000000 0 0
usbphy_k 1 1 24000000 0 0
ck_per 1 1 24000000 0 0
adc12_k 1 1 24000000 0 0
ref4 1 1 24000000 0 0
pll4 1 1 594000000 0 0
pll4_r 0 0 74250000 0 0
pll4_q 1 1 31263158 0 0
ltdc_px 1 1 31263158 0 0
dsi_px 0 0 31263158 0 0
fdcan_k 0 0 31263158 0 0
I'm thinking that maybe the FDCAN clock is not activated when I turn on the board in production mode
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.