2025-07-02 2:29 PM
Hi Team,
I am able to test FDCAN1 on M33 core of STM32MP257F EV1 board, using STM32Cube\Repository\STM32Cube_FW_MP2_V1.1.0\Projects\STM32MP257F-EV1\Examples\FDCAN\FDCAN_Com_IT and PEAK PCAN Usb.
However, when I try to change the same code to work for FDCAN2, I couldn't achieve it. as A35 core is going to reset, probably due to wrong call to Resource Manager. Below is the snippet of code used.
/* Acquire FDCAN using Resource manager */
if (RESMGR_STATUS_ACCESS_OK == ResMgr_Request(RESMGR_RESOURCE_RIFSC, STM32MP25_RIFSC_FDCAN_ID))
{
/* Enable FDCANx clock */
FDCANx_CLK_ENABLE();
}
/* Acquire GPIOJ14 using Resource manager */
if (RESMGR_STATUS_ACCESS_OK != ResMgr_Request(RESMGR_RESOURCE_RIF_GPIOJ, RESMGR_GPIO_PIN(14)))
{
Error_Handler();
}
/* Acquire GPIOI12 using Resource manager */
if (RESMGR_STATUS_ACCESS_OK != ResMgr_Request(RESMGR_RESOURCE_RIF_GPIOI, RESMGR_GPIO_PIN(12)))
{
Error_Handler();
}
/* Enable GPIOs power supplies */
if (RESMGR_STATUS_ACCESS_OK == ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, RESMGR_RCC_RESOURCE(96)))
{
FDCANx_TX_GPIO_CLK_ENABLE();
FDCANx_RX_GPIO_CLK_ENABLE();
}
Below are my observations,
Also, it looks like Ports I12 and J14 are mapped to FDCAN3 on STM32MP2 controller, however on the EV1 board, the CAN channel (CN11) is called FDCAN2. Please clarify if the CN11 DB9 is FDCAN2 or FDCAN3.
It would be helpful, if I can get a working M33 code that is tested for FDCAN2 (CN11 DB-9 port) also.
Best Regards,
Venkata
2025-07-07 6:05 AM
Hi Venkata,
/* Enable GPIOs power supplies */
>if (RESMGR_STATUS_ACCESS_OK == ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, >RESMGR_RCC_RESOURCE(96)))
>{
>FDCANx_TX_GPIO_CLK_ENABLE();
>FDCANx_RX_GPIO_CLK_ENABLE();
>}
I think the RCC peripheral indicated by "RESMGR_RCC_RESOURCE(96)" indicates GPIOG.
(CANFD1 uses GPIOG only )
See
Table 39. Indexes for RIF-aware peripherals (with RCC control index) in
STM32MP23/25xx advanced Arm<Sup>®</Sup>-based 32/64-bit MPUs - Reference manual
So. you may change
If you use GPIOJ and GPIOI.
How about trying the following?
ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, RESMGR_RCC_RESOURCE(98)) //GPIOI
ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, RESMGR_RCC_RESOURCE(99)) //GPIOJ
e.g.
/* Enable GPIOs power supplies */
if (RESMGR_STATUS_ACCESS_OK == ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, RESMGR_RCC_RESOURCE(98)))
{
FDCANx_RX_GPIO_CLK_ENABLE();
}
if (RESMGR_STATUS_ACCESS_OK == ResMgr_Request(RESMGR_RESOURCE_RIF_RCC, RESMGR_RCC_RESOURCE(99)))
{
FDCANx_TX_GPIO_CLK_ENABLE();
}
Hope it help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.