2020-11-20 11:45 AM
STM32MP157-DK2 with Buildroot image.
I'm running a Qt app on the A7 core and using QSerial to talk to the M4 core using OpenAMP to talk through ttyRPMSG0. Right now it takes ~10ms to send/receive from Qt to M4. Is there anything I can do to decrease this time to say 1ms?
The ttyRPMSG0 port has a baud rate of 38400, but I don't see a way to increase that.
Any ideas would be appreciated.
Solved! Go to Solution.
2020-11-26 12:59 AM
Hi @shane mattner ,
If you have a big amount of data to transfert, the following wiki article could help to improve performances : How to exchange large data buffers with the coprocessor - example.
BR,
Christophe
2020-11-26 12:59 AM
Hi @shane mattner ,
If you have a big amount of data to transfert, the following wiki article could help to improve performances : How to exchange large data buffers with the coprocessor - example.
BR,
Christophe
2020-11-26 5:42 AM
Great article, thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.