2019-07-14 8:16 PM
I'd like to test the standby mode on the board STM32MP157C-DK2,so I run the application 'OpenAMP_TTY_echo_wakeup' by following the doc -- readme.txt in STM32Cube MP1 package. However ,once I run the command
$ echo mem > /sys/power/stateto move CA7 in CStop mode , it will report such error:
[ 281.518965] PM: Syncing filesystems ... done.
[ 281.546418] Freezing user space processes ... (elapsed 0.001 seconds) done.
[ 281.553742] OOM killer disabled.
[ 281.557176] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
[ 281.564607] Suspending console(s) (use no_console_suspend to debug)
[ 281.629016] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget
[ 281.629035] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0
[ 281.629045] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0
[ 281.694403] stm32-dma 48001000.dma: Suspend is prevented by Chan 1
[ 281.694436] dpm_run_callback(): platform_pm_suspend+0x0/0x48 returns -16
[ 281.694447] PM: Device 48001000.dma failed to suspend: error -16
[ 281.694458] PM: Some devices failed to suspend, or early wake event detected
[ 281.705449] dwmac4: Master AXI performs any burst length
[ 281.705484] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 281.747812] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget
[ 282.290600] OOM killer enabled.
[ 282.293712] Restarting tasks ... done.
[ 282.344351] PM: suspend exit
-sh: echo: write error: Device or resource busy
Do you know the reason for this problem?
Solved! Go to Solution.
2019-09-18 1:10 PM
I got the same error like you but I couldn't solve the problem so far. How did you switch between engineering boot mode and production boot mode ? Do you mean the eclipse debug configuration tab in the attachment ?
other question : Our scenario is the second scenario in the readme file. There it says "Set Exti line 61 (IPCC interrupt CPU1) as source of wakeup". So I modified the code and changed 62 to 61 and some other lines related. Did you modify your code as well ? If yes, could you please send me modified codes if possible.
I will appricate a possible answer very muc, thanks a lot !
2019-09-18 11:29 PM
Engineering mode set in SW4STM32 should be also set on the board using BOOT[2:0] = 0b100
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.