2020-03-31 1:10 AM
I downloaded, installed and configured Eclipse, Version: 2020-03 (4.15.0), UBUNTU 16.04 LTS
Wrote a simple program:
#include <stdio.h>
#include <stdlib.h>
int main(void)
{
printf( "Hello world\n" );
return 1;
}
compiles without errors :)
But, when I run on the board, it gives an error:
Inconsistency detected by ld.so: dl-lookup.c: 948: _dl_setup_hash: Assertion `(bitmask_nwords & (bitmask_nwords - 1)) == 0' failed!
if I compile this program, as shown in the example in the Wiki "Create a simple hello-world application", then everything works fine.
i think something with eclipse settings.
Did anyone have this?
Sincerely, Alexander
2020-03-31 7:57 AM
Hello Alexander,
I'm sorry - in my previous reply I didn't provide correct info.
By mistake I copied settings from another project.
Try following linker settings in Miscellaneous -> Linker flags
-mfloat-abi=hard -mtune=cortex-a7 --sysroot=/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Let me know if it works now
BR,
Milan
2020-03-31 11:50 PM
Hello Milan!
thanks for the answer
I tried with new linker flags.
Unfortunately, the same error again :(
maybe it's because i use STM32MP15-Ecosystem-v1.1.0 ?
best regards
Alexander
2020-04-01 1:45 AM
Hello Alexander,
I use 1.2.0 but I don't think it's the real issue.
Could you provide result of comp / linker?
BR,
Milan
2020-04-01 4:50 AM
2020-04-03 4:40 AM
Hello Milan!
I found that the object file 222.o is working correctly
if you run it on the DK2 board, it works fine :)
I think the linker is not working properly
setting for compiler: -I/home/alexsander/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/include -O0 -g3 -Wall --sysroot=/home/alexsander/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7
setting for linker: -nostartfiles --sysroot=/home/alexsander/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -mfloat-abi=hard -mtune=cortex-a7
in the attachment, the object file 222.о
I renamed it 222
may need to change linker settings?
best regards
Alexander
2020-04-07 3:58 AM
Hello Alexander,
In you first sentence you write that the result in working fine on DK2.
I guess you can execute it on the board.
If this si right, what's the issue with linker?
Best regards,
Milan
2020-04-07 4:30 AM
Hello Milan!
i think you're right
linker is not working properly
i don't know how to fix it :(
best regards
Alexander
2020-04-08 9:09 AM
Hi Alexander,
sorry for misunderstanding, but on my side both link and compiler work properly.
Could you send log of compiler and linker?
make all
Building file: /home/osboxes/STM32MP15-Ecosystem-v1.2.0/Developer-Package/stm32mp1-openstlinux-20-02-19/sources/gtk_hello_world_example/gtk_hello_world.c
Invoking: Cross GCC Compiler
arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/gtk-3.0/ -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/glib-2.0/include/ -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/glib-2.0/ -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/glib-2.0/ -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/at-spi2-atk/2.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/at-spi-2.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/dbus-1.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/dbus-1.0/include -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/gio-unix-2.0/ -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/cairo -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/libdrm -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/pango-1.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/harfbuzz -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/pango-1.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/fribidi -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/atk-1.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/cairo -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/pixman-1 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/freetype2 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/libpng16 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/gdk-pixbuf-2.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/libpng16 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/glib-2.0 -I/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/glib-2.0/include -O0 -g3 -Wall -c -fmessage-length=0 --sysroot=/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -MMD -MP -MF"gtk_hello_world.d" -MT"gtk_hello_world.o" -o "gtk_hello_world.o" "/home/osboxes/STM32MP15-Ecosystem-v1.2.0/Developer-Package/stm32mp1-openstlinux-20-02-19/sources/gtk_hello_world_example/gtk_hello_world.c"
Finished building: /home/osboxes/STM32MP15-Ecosystem-v1.2.0/Developer-Package/stm32mp1-openstlinux-20-02-19/sources/gtk_hello_world_example/gtk_hello_world.c
Building target: cross_trial
Invoking: Cross GCC Linker
arm-ostl-linux-gnueabi-gcc -L/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/lib/ -mfloat-abi=hard -mtune=cortex-a7 --sysroot=/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi -o "cross_trial" ./gtk_hello_world.o -lgtk-3 -lgdk-3 -lpangocairo-1.0 -lpango-1.0 -latk-1.0 -lcairo-gobject -lcairo -lgdk_pixbuf-2.0 -lgio-2.0 -lgobject-2.0 -lglib-2.0
Finished building target: cross_trial
I will check your settings,
BR,
Milan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.