STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

add WLAN interface to stm32mp157f-dk2

Hi ST Community,I have been trying to add the WLAN interface to my stm32mp157f-dk2 board with the distro "openstlinux-weston" and the machine "stm32mp1" without success with the following documentation:I have applied the kernel configuration given in...

FBofi.1 by Associate II
  • 9444 Views
  • 8 replies
  • 0 kudos

Resolved! STM32MP1 cannot read M4 message

Hi! I have created a program to send messages between cores (A7 and M4), using virtual uart. The messages that are sent from the A7 core are received by the M4 core. My error occurs when I try to read the messages that are sent from the M4 core to th...

0693W00000WIgaeQAD.png
TArre.1 by Associate III
  • 1840 Views
  • 4 replies
  • 0 kudos

Want to turn off thermal shutdown at 120C on STM32MP157A-DK1 to test it at higher temperatures

Hello, I would like to disable the thermal shutdown at 120C on STM32MP157A-DK1 which embeds a STM32MP157A. It runs Yocto Project and contrary to other boards I worked on, I cannot turn off and even change the critical temperature (the procedure is th...

ACard.1 by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

Why num_of_vrings is set to 0 if I start M4 code with spl and why is it set to 2 when I start code with linux?

Hi,I'm using stm32mp153c and I managed to start M4 code after the SPL initialization and before U-BOOT. All initializations work fine except for the MX_OPENAMP_Init.I see that if I start the code after SPL the variable of num_of_vrings (that is equa...

ASega.1 by Associate III
  • 1594 Views
  • 1 replies
  • 0 kudos

TF-A VDD and phandle errors

Hi, I have upgraded to Ecosystem 3.1.1 and have started to get warnings in TF-A when booting up my stm32mp151c. These are the warnings: NOTICE: CPU: STM32MP151CAA Rev.B NOTICE: Model: STMicroelectronics custom STM32CubeMX board NOTICE: Bootrom aut...

JMour.2 by Associate II
  • 2324 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.